2024-09-26 4:57 AM
Hi,
is it possible to swap the DSI lanes so that lane 0 becomes lane 1 and the other way around? This would simplify routing on our PCB. I've found there are configuration bits in the DSI_WPCR0 register for custom lane configuration (SWDL0 and SWDL1), but as far as I understood, these can only swap the pin order within a lane. Have I overlooked something or is the STM32MP157 not capable of swapping lanes?
Best regards,
Robert
Solved! Go to Solution.
2024-09-27 7:35 AM
Hi @rtie
I confirm your analyse.
DSI clock or a data lane uses 2 physical pins (+ and -) and bits in DSI_WPCR0 registers can be used to "swap" these + and - pins. Unfortunately, it is not possibe to swap data lane 0 pins with data lane 1 pins.
Olivier
2024-09-27 7:35 AM
Hi @rtie
I confirm your analyse.
DSI clock or a data lane uses 2 physical pins (+ and -) and bits in DSI_WPCR0 registers can be used to "swap" these + and - pins. Unfortunately, it is not possibe to swap data lane 0 pins with data lane 1 pins.
Olivier
2024-09-30 4:02 AM
OK, thank you very much for the confirmation!
Robert
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.