2020-03-31 12:53 PM
Hello,
I'm trying to connect stm32mp157c-dk2 board with another device over FDCAN in engineering mode (MCU single core) using CN2 pin 3 and 5 (stm32 PA12 and PA11 pins respectively). Though I can initialize and request to use FDCAN1 from resource manager utility without any error, FDCAN related interrupts still don't get fired. Do I need to assign RX/TX pins to M4 FDCAN1 in tf-a, u-boot or kernel device trees.
Solved! Go to Solution.
2020-04-01 1:39 AM
Hi @MNoor.1
In Engeneering mode A7 is on hold and M4 is able to initialize the assigned IPs as per configured in CubeMX.
Thus, not need to change anything on Linux side. ( have to be done when you will move to Production mode)
I guess you should check your FDCAN and related IT settings in CubeMX.
Olivier
2020-04-01 1:39 AM
Hi @MNoor.1
In Engeneering mode A7 is on hold and M4 is able to initialize the assigned IPs as per configured in CubeMX.
Thus, not need to change anything on Linux side. ( have to be done when you will move to Production mode)
I guess you should check your FDCAN and related IT settings in CubeMX.
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.