cancel
Showing results for 
Search instead for 
Did you mean: 

DDR tuning fails Bit Deskew and Eye Training

TStru.1
Associate II

I'm DDR tuning a custom STM32MP157F board with 4GB DDR3. All DDR tests are passing however I get the following tuning failure for Bit Deskew: Failed [Cannot Deskew lines, there is no PASS region] and Eye Training: [Cannot DQS timings, there is no PASS region]

What exactly does this mean? How can it fail tuning but pass testing?

DDR>test 0
...
loop 1: 0/17 test failed
 
Result: Pass [loop 1: 17 tests passed]
DDR>tuning 1
execute 1:Bit de-skew
Result: Failed [Cannot Deskew lines, there is no PASS region]
Result: Failed [Cannot Deskew lines, there is no PASS region]
Result: Failed [error = 2]
DDR>tuning 2
execute 2:Eye Training
Result: Failed [Cannot DQS timings, there is no PASS region]
Byte 1, DQS unit = 3, phase = 3
Result: Failed [error = 1]
DDR>tuning 3
execute 3:Display registers
Byte 0 Dekew result, bit0 delay, bit1 delay...bit8 delay
  2 2 2 2 2 2 2 2 
dxndllcr: [5a0041cc] val:400a0000
dxnqdstr: [5a0041d4] val:3db02001
dxndqtr: [5a0041d0] val:aaaaaaaa
Byte 1 Dekew result, bit0 delay, bit1 delay...bit8 delay
  2 2 2 2 2 2 2 2 
dxndllcr: [5a00420c] val:40000000
dxnqdstr: [5a004214] val:3db02001
dxndqtr: [5a004210] val:aaaaaaaa
Result: Pass []
DDR>tuning 4
execute 4:Bist config
Bist.nbErr = 1
Bist.Seed = 0x1234abcd
Result: Pass []

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
OlivierK
ST Employee

Hello ​TStru.1 (Community Member) 

An issue has been identified regarding DQS Gating (function call missing) and will be corrected in next release of CubeMx/DDR tool (v6.3)

You still can run DDR tool and apply the calibration values from the test, but you'll need to update 4 registers manually if you want to include the DQS values in the DT.

https://wiki.st.com/stm32mpu/wiki/DDRCTRL_and_DDRPHYC_device_tree_configuration

In my case (16-bit DDR)

DDR>step 3         

current step is 3:DDR_READY             

DDR>tuning 0                                  

execute 0:Read DQS gating                            

Byte 0, R0DGSL = 2, R0DGPS = 0                         

Byte 1, R0DGSL = 2, R0DGPS = 0                         

Result: Pass []

-> According to the DQS gating above and the corresponding table (shown below), I need to update manually DX0DQSTR, DX1DQSTR as follow

DX0DQSTR 0x3DB00002  

DX1DQSTR 0x3DB00002 

For a 32-bit DDR (in your case) you will have also Byte2, Byte3 showing values.

update manually the 4 registers : DX0DQSTR/DX1DQSTR/DX2DQSTR/DX3DQSTR

Here's the corresponding table to update the registers according to DQS values:

Example for Byte 0 with all combinations from DQS Gating,

( same table for Byte1 = DX1DQSTR, Byte2 = DX2DQSTR, Byte3 =DX3DQSTR)  

Byte 0, R0DGSL = 0, R0DGPS = 0 => DX0DQSTR = 0x3DB00000

Byte 0, R0DGSL = 0, R0DGPS = 1 => DX0DQSTR = 0x3DB01000

Byte 0, R0DGSL = 0, R0DGPS = 2 => DX0DQSTR = 0x3DB02000

Byte 0, R0DGSL = 0, R0DGPS = 3 => DX0DQSTR = 0x3DB03000

Byte 0, R0DGSL = 1, R0DGPS = 0 => DX0DQSTR = 0x3DB00001

Byte 0, R0DGSL = 1, R0DGPS = 1 => DX0DQSTR = 0x3DB01001

Byte 0, R0DGSL = 1, R0DGPS = 2 => DX0DQSTR = 0x3DB02001

Byte 0, R0DGSL = 1, R0DGPS = 3 => DX0DQSTR = 0x3DB03001

Byte 0, R0DGSL = 2, R0DGPS = 0 => DX0DQSTR = 0x3DB00002

Byte 0, R0DGSL = 2, R0DGPS = 1 => DX0DQSTR = 0x3DB01002

Byte 0, R0DGSL = 2, R0DGPS = 2 => DX0DQSTR = 0x3DB02002

Byte 0, R0DGSL = 2, R0DGPS = 3 => DX0DQSTR = 0x3DB03002

Byte 0, R0DGSL = 3, R0DGPS = 0 => DX0DQSTR = 0x3DB00003

Byte 0, R0DGSL = 3, R0DGPS = 1 => DX0DQSTR = 0x3DB01003

Byte 0, R0DGSL = 3, R0DGPS = 2 => DX0DQSTR = 0x3DB02003

Byte 0, R0DGSL = 3, R0DGPS = 3 => DX0DQSTR = 0x3DB03003

Byte 0, R0DGSL = 4, R0DGPS = 0 => DX0DQSTR = 0x3DB00004

Byte 0, R0DGSL = 4, R0DGPS = 1 => DX0DQSTR = 0x3DB01004

Byte 0, R0DGSL = 4, R0DGPS = 2 => DX0DQSTR = 0x3DB02004

Byte 0, R0DGSL = 4, R0DGPS = 3 => DX0DQSTR = 0x3DB03004

Byte 0, R0DGSL = 5, R0DGPS = 0 => DX0DQSTR = 0x3DB00005

Byte 0, R0DGSL = 5, R0DGPS = 1 => DX0DQSTR = 0x3DB01005

Byte 0, R0DGSL = 5, R0DGPS = 2 => DX0DQSTR = 0x3DB02005

Byte 0, R0DGSL = 5, R0DGPS = 3 => DX0DQSTR = 0x3DB03005

Byte 0, R0DGSL = 6, R0DGPS = 0 => DX0DQSTR = 0x3DB00006

Byte 0, R0DGSL = 6, R0DGPS = 1 => DX0DQSTR = 0x3DB01006

Byte 0, R0DGSL = 6, R0DGPS = 2 => DX0DQSTR = 0x3DB02006

Byte 0, R0DGSL = 6, R0DGPS = 3 => DX0DQSTR = 0x3DB03006

Byte 0, R0DGSL = 7, R0DGPS = 0 => DX0DQSTR = 0x3DB00007

Byte 0, R0DGSL = 7, R0DGPS = 1 => DX0DQSTR = 0x3DB01007

Byte 0, R0DGSL = 7, R0DGPS = 2 => DX0DQSTR = 0x3DB02007

Byte 0, R0DGSL = 7, R0DGPS = 3 => DX0DQSTR = 0x3DB03007


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
OlivierK
ST Employee

Hello ​TStru.1 (Community Member) 

An issue has been identified regarding DQS Gating (function call missing) and will be corrected in next release of CubeMx/DDR tool (v6.3)

You still can run DDR tool and apply the calibration values from the test, but you'll need to update 4 registers manually if you want to include the DQS values in the DT.

https://wiki.st.com/stm32mpu/wiki/DDRCTRL_and_DDRPHYC_device_tree_configuration

In my case (16-bit DDR)

DDR>step 3         

current step is 3:DDR_READY             

DDR>tuning 0                                  

execute 0:Read DQS gating                            

Byte 0, R0DGSL = 2, R0DGPS = 0                         

Byte 1, R0DGSL = 2, R0DGPS = 0                         

Result: Pass []

-> According to the DQS gating above and the corresponding table (shown below), I need to update manually DX0DQSTR, DX1DQSTR as follow

DX0DQSTR 0x3DB00002  

DX1DQSTR 0x3DB00002 

For a 32-bit DDR (in your case) you will have also Byte2, Byte3 showing values.

update manually the 4 registers : DX0DQSTR/DX1DQSTR/DX2DQSTR/DX3DQSTR

Here's the corresponding table to update the registers according to DQS values:

Example for Byte 0 with all combinations from DQS Gating,

( same table for Byte1 = DX1DQSTR, Byte2 = DX2DQSTR, Byte3 =DX3DQSTR)  

Byte 0, R0DGSL = 0, R0DGPS = 0 => DX0DQSTR = 0x3DB00000

Byte 0, R0DGSL = 0, R0DGPS = 1 => DX0DQSTR = 0x3DB01000

Byte 0, R0DGSL = 0, R0DGPS = 2 => DX0DQSTR = 0x3DB02000

Byte 0, R0DGSL = 0, R0DGPS = 3 => DX0DQSTR = 0x3DB03000

Byte 0, R0DGSL = 1, R0DGPS = 0 => DX0DQSTR = 0x3DB00001

Byte 0, R0DGSL = 1, R0DGPS = 1 => DX0DQSTR = 0x3DB01001

Byte 0, R0DGSL = 1, R0DGPS = 2 => DX0DQSTR = 0x3DB02001

Byte 0, R0DGSL = 1, R0DGPS = 3 => DX0DQSTR = 0x3DB03001

Byte 0, R0DGSL = 2, R0DGPS = 0 => DX0DQSTR = 0x3DB00002

Byte 0, R0DGSL = 2, R0DGPS = 1 => DX0DQSTR = 0x3DB01002

Byte 0, R0DGSL = 2, R0DGPS = 2 => DX0DQSTR = 0x3DB02002

Byte 0, R0DGSL = 2, R0DGPS = 3 => DX0DQSTR = 0x3DB03002

Byte 0, R0DGSL = 3, R0DGPS = 0 => DX0DQSTR = 0x3DB00003

Byte 0, R0DGSL = 3, R0DGPS = 1 => DX0DQSTR = 0x3DB01003

Byte 0, R0DGSL = 3, R0DGPS = 2 => DX0DQSTR = 0x3DB02003

Byte 0, R0DGSL = 3, R0DGPS = 3 => DX0DQSTR = 0x3DB03003

Byte 0, R0DGSL = 4, R0DGPS = 0 => DX0DQSTR = 0x3DB00004

Byte 0, R0DGSL = 4, R0DGPS = 1 => DX0DQSTR = 0x3DB01004

Byte 0, R0DGSL = 4, R0DGPS = 2 => DX0DQSTR = 0x3DB02004

Byte 0, R0DGSL = 4, R0DGPS = 3 => DX0DQSTR = 0x3DB03004

Byte 0, R0DGSL = 5, R0DGPS = 0 => DX0DQSTR = 0x3DB00005

Byte 0, R0DGSL = 5, R0DGPS = 1 => DX0DQSTR = 0x3DB01005

Byte 0, R0DGSL = 5, R0DGPS = 2 => DX0DQSTR = 0x3DB02005

Byte 0, R0DGSL = 5, R0DGPS = 3 => DX0DQSTR = 0x3DB03005

Byte 0, R0DGSL = 6, R0DGPS = 0 => DX0DQSTR = 0x3DB00006

Byte 0, R0DGSL = 6, R0DGPS = 1 => DX0DQSTR = 0x3DB01006

Byte 0, R0DGSL = 6, R0DGPS = 2 => DX0DQSTR = 0x3DB02006

Byte 0, R0DGSL = 6, R0DGPS = 3 => DX0DQSTR = 0x3DB03006

Byte 0, R0DGSL = 7, R0DGPS = 0 => DX0DQSTR = 0x3DB00007

Byte 0, R0DGSL = 7, R0DGPS = 1 => DX0DQSTR = 0x3DB01007

Byte 0, R0DGSL = 7, R0DGPS = 2 => DX0DQSTR = 0x3DB02007

Byte 0, R0DGSL = 7, R0DGPS = 3 => DX0DQSTR = 0x3DB03007


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.