STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I change device tree?

I understand that when I create my own machine, I can create device tree by following 2 method. Method 1) Building device trees by Developer Package (separately from bitbake) This method is described in following Wiki page. https://wiki.st.com/stm32m...

HMasu.1 by Senior
  • 3296 Views
  • 5 replies
  • 0 kudos

OpenAMP Linux Side

Hi,iam trying to get an understanding of the OpenAMP Framework and i wanna use it for interprocess communication with the STM32MP1. As my understanding, the OpenAMP Framework could be used from Baremetal/RTOS side and apparently also from Linux Side....

YRink.1 by Associate II
  • 3327 Views
  • 3 replies
  • 1 kudos

Resolved! Using KSZ8794 with STM32MP151C

Hello,we have a custom board based on STM32MP151C. On our SPI is the Ethernet Switch KSZ8794. How should I proceed to enable the ethernet in the U-Boot? I have already configured the etherne0 node (according to the ST documentation). Should I add the...

alenik-mm by Associate II
  • 2314 Views
  • 1 replies
  • 0 kudos

Can I connect any other Wi-Fi module in place of 1DX? If yes, is there a clean way to achieve this?

I am interested in the platform to evaluate wifi chips from different vendors. But based on the quick run through schematic, I don't think its possible to connect any different wifi chip (which has sdio as supported interface) in the DK2 kit. If anyo...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.