2022-11-09 3:03 AM - last edited on 2023-06-16 5:53 AM by Kevin HUBER
Hi,
Can we use a DDR3L from Winbond with part number W634GU6NB-11 (Speed bin 1866) with STMPU STM32MP1ADD3.
As STM32MP1 datasheet suggest that it can support up-to 1066. So using above part from Winbond will have any interface issue ?
Thanks.
Hi @Community member
can you please share your input on above issue.
Solved! Go to Solution.
2022-11-09 4:48 AM
Hi @PS.2
Faster memory could work at slower frequency.
Will likely work with default DDR3L-1066 conservative settings. Please look at AN5168 for details of configuration choices which could probably enhance a bit the performances (CL improvement gain is usually barely noticeable at system level, especially on x32 DDR).
Regards.
2022-11-09 4:48 AM
Hi @PS.2
Faster memory could work at slower frequency.
Will likely work with default DDR3L-1066 conservative settings. Please look at AN5168 for details of configuration choices which could probably enhance a bit the performances (CL improvement gain is usually barely noticeable at system level, especially on x32 DDR).
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.