2020-05-01 8:11 AM
Can i connect J-Link to test points TP2,TP3,TP4,TP5,TP8,TP9 and not use the embedded ST-Link/V2 ? If yes do it needs special treatment like disabling embedded ST-Link/V2 ?
2020-05-03 11:51 PM
Hello,
Yes, you could use these points for an external probe.
Should work without specific embedded ST-Link disable (obviously, to avoid conflicts, you must not start any debugging session on ST-Link), and you could still use UART4 VCP thru ST-Link USB.
Please ensure you have the latest ST-Link FW.
Anyway, In case of trouble, you could totally disable ST-Link (debug and VCP) using SB18, or just disconnect ST-Link SWD wires using SB17, SB19 and SB20.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.