2020-11-25 1:51 AM
Hello totgehet,
i wanted to build a Kernelmodule for my Projekt so i started to install the SDK and wrote a simple Programm to see if i can make a Programm in the userspace. This works fine. My next step was to Building and deploying the Linux kernel. For that I followed the installation https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package. But when I want to Compile and install on a build directory I get this error from the makefil:
make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040 O="$PWD/../build"
make[1]: Entering directory '/opt/st/stm32mp1/3.1-openstlinux-5.4-dunfell-mp1-20-11-12/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0/build'
GEN Makefile
scripts/kconfig/conf --syncconfig Kconfig
GEN Makefile
SYSHDR arch/arm/include/generated/uapi/asm/unistd-common.h
SYSHDR arch/arm/include/generated/uapi/asm/unistd-oabi.h
SYSHDR arch/arm/include/generated/uapi/asm/unistd-eabi.h
HOSTCC scripts/dtc/dtc.o
HOSTCC scripts/dtc/flattree.o
HOSTCC scripts/dtc/fstree.o
HOSTCC scripts/dtc/data.o
HOSTCC scripts/dtc/livetree.o
HOSTCC scripts/dtc/treesource.o
HOSTCC scripts/dtc/srcpos.o
HOSTCC scripts/dtc/checks.o
HOSTCC scripts/dtc/util.o
LEX scripts/dtc/dtc-lexer.lex.c
YACC scripts/dtc/dtc-parser.tab.[ch]
HOSTCC scripts/dtc/dtc-lexer.lex.o
HOSTCC scripts/dtc/dtc-parser.tab.o
HOSTCC scripts/dtc/yamltree.o
HOSTLD scripts/dtc/dtc
HOSTCC scripts/genksyms/genksyms.o
YACC scripts/genksyms/parse.tab.[ch]
HOSTCC scripts/genksyms/parse.tab.o
LEX scripts/genksyms/lex.lex.c
HOSTCC scripts/genksyms/lex.lex.o
HOSTLD scripts/genksyms/genksyms
HOSTCC scripts/kallsyms
HOSTCC scripts/conmakehash
HOSTCC scripts/sortextable
HOSTCC scripts/asn1_compiler
HOSTCC scripts/sign-file
/opt/st/stm32mp1/3.1-openstlinux-5.4-dunfell-mp1-20-11-12/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0/linux-5.4.56/scripts/sign-file.c:25:10: fatal error: openssl/opensslv.h: No such file or directory
25 | #include <openssl/opensslv.h>
| ^~~~~~~~~~~~~~~~~~~~
compilation terminated.
make[2]: *** [scripts/Makefile.host:107: scripts/sign-file] Error 1
make[1]: *** [/opt/st/stm32mp1/3.1-openstlinux-5.4-dunfell-mp1-20-11-12/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0/linux-5.4.56/Makefile:1100: scripts] Error 2
make[1]: Leaving directory '/opt/st/stm32mp1/3.1-openstlinux-5.4-dunfell-mp1-20-11-12/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0/build'
I checked my SDK and I saw that the Headerfile is available. This is why I have no idea how to fix the build. I hope someone can help me Thanks so far.
Solved! Go to Solution.
2020-11-25 2:09 AM
It seems like you need OpenSSL development package on your PC. Try this:
$ sudo apt-get install libssl-dev
2020-11-25 2:09 AM
It seems like you need OpenSSL development package on your PC. Try this:
$ sudo apt-get install libssl-dev
2020-11-25 2:39 AM
Hi @SAman.1 ,
Thanks @JYune you are right
To be complete pay attention to install all extra package as per listed here :
https://wiki.st.com/stm32mpu/wiki/PC_prerequisites#Install_extra_packages
Olivier
2020-11-25 5:03 AM
Thanks now its working i already compiled a simple kernel module.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.