2024-08-05 7:16 AM
Hi,
I am currently working on a project that requires us to install a browser on our board. We are using an STM32mp25, which is using the Mickledore image. I am finding that the meta-browser layer is not compatible with Mickledore, and if I'm not mistaken meta-browser only runs on Scarthgap. What I've tried to do is switch my layers to the Scarthgap branch, and unfortunately what I find is that from my conf/local.conf is that the stm32mp25 is not a recognized maching (MACHINE = "stm32pm25"), meaning that the stm32mp25 is not supported on Scarthgap.
Has anyone successfully installed a browser on the stm32mp25 (eval board)? Any help would be greatly appreciated!
For reference I was following along with this demo https://www.digikey.com/en/maker/projects/intro-to-embedded-linux-part-2-yocto-project/2c08a1ad09d74f20b9844e566d332da4
Solved! Go to Solution.
2024-08-09 9:02 AM
Hi @mdivertie
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
2024-08-05 8:00 AM
Hi @mdivertie,
Scarthgap is not yet supported by ST delivery. It's plan on the next DV planned for Q4.
regards,
Grégory
2024-08-06 10:21 AM
How could we support a browser (Chromium/Firefox) in the meantime?
2024-08-06 11:53 PM
Hi @mdivertie,
I think you can refer to this forum post to install a browser on MP15 : https://community.st.com/t5/stm32-mpus-embedded-software/qt-wpe-simple-browser-installation-failed/td-p/703413
Regards,
Grégory
2024-08-09 1:11 AM
Hi @mdivertie,
Today, there is no official support of Chromium for STM32MP25. It might append by the end of the year.
Internally, we have tried Qt6 webengine that includes Chromium (meta-qt6 layer). Today, there are some performance limitations (some GPU or HW video acceleration are missing) that can lead to a bad user experience. But in kiosk mode and for specific web sites, browsing can be done correctly.
For additional technical info, please contact STM support.
BR,
Philippe.
2024-08-09 9:02 AM
Hi @mdivertie
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
2024-10-28 8:18 PM
2024-10-31 7:10 AM
Hi Melody,
Yes, we were able to install a browser on an stm32Mp2. A colleague used this recipe
Best,
Matt
2024-11-02 4:52 AM
Thank you Matt!
So must build the whole os using Yocto. There isn't a package to install to the existing system, right?
And have u also tried a browser on X11 distro? Thank you!
2025-06-09 10:47 AM
I'm very intrested of the status of this thread. Is it working now? Lag free browsing at 1080p at Youtube or other?
I'm building a custom board of STM32MP257FAK3 processor. My goal is to use the MP2 as mini-PC for streaming in 1080p. Youtube/GeForce Now by using Chromium.
Yes I know that MP2 is not meant to be used as a mini-PC. Even if it could be used as a mini-PC.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.