STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Fast Boot Mode

Hello everyone,for the board TXMP1570 in Fast boot mode I am looking for the corresponding driver "USB download gadget" Win 11, VID_0483&PID_5720. Thanks in advance Marko

MP2 by Associate II
  • 3750 Views
  • 6 replies
  • 0 kudos

Resolved! Fried SIP with external power

I am currently working on bringing up a production board design with the OSD32MP157C-512M-IAA. The board is by design very similar to the Octavo systems osd32mp1-red board and the USB part is very similar to ST STM32MP157-EVAL where VBUS pin in uUSB ...

Henrik1 by Associate
  • 1555 Views
  • 1 replies
  • 1 kudos

Prepare kernel source

Hello, I'm trying modify device tree following this website :STM32MPU Developer Package - stm32mputhan now Im working on :meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp/README.HOW_TO.txt at mickledore · STMicroelectronics/meta-st-stm32mp · GitHub...

2024-07-11_10h21_02.png

Transmit Videostream - FPV

Hello everyone,We are at the beginning of the development phase for creating FPV-drones.I would like to transmit the video signal (FPV) of a camera, e.g. the RPI-22 camera, via radio over a distance of 2 km or more from the STM32MP25x-EV1 evaluation ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.