STM32MP OpenCV installation
Hello,My aim is to install OpenCV and use it's functionalities on STM32MP1 board. But I coulnd't find a proper documentation about it. Could you help me with this?Thanks.
Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.
Hello,My aim is to install OpenCV and use it's functionalities on STM32MP1 board. But I coulnd't find a proper documentation about it. Could you help me with this?Thanks.
I generated the M33 code using CubeIDE by following the lab manual.During the driver initializations:MX_ADC1_Init();MX_I2C1_Init();MX_ICACHE_Init();MX_RTC_Init();The A35 halts CPU1 and resets after sometime.E/TC:0 stm32_iac_itr:192 IAC exceptions [15...
NOTICE: CPU: STM32MP135F Rev.YNOTICE: Model: STMicroelectronics STM32MP135F-DK STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mp1-v23.06.21NOTICE: BL2: v2.8-stm32mp1-r1.0(release):custom()NOTICE: BL2: Built : 15:38:01, Jul 2 2025NOTICE: BL2: Bo...
Hi everyone,I'm working with the STM32MP157C-DK2 board and trying to reduce the amount of RAM allocated to OP-TEE, but so far I haven't been successful.There are 32MiB DDR dedicated for OP-TEE. 30MiB for TZSRAM and 2MiB for SHMEM.In OP-TEE sources I ...
I am able to use FDCAN1 to communicate on the A7 by adding the following to `STM32MPU-Ecosystem-v6.0.0/Developer-Package/stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sources/arm-ostl-linux-gnueabi/linux-stm32mp-6.6.48-stm32mp-r1-r0/linux-6....
Hi STM Team,We are working with a custom board based on the STM32MP157DAC.We are facing a video lag issue when trying to play a video file from Qt application 6.5.3 using media player.Even reducing the frame rate had no effect.But if we use gst-play ...
Hello,I'm using Buildroot environment with the STM32MP257F-DK board. I'm testing GStreamer with a simple pipeline:gst-launch-1.0 videotestsrc ! autovideosinkWhen I first run it there is no problem. The test video shows fine on the HDMI monitor. But w...
I am using a custom board (STM32MP157DAA1) and want to use DSI 1 lane. How do I set it up in uboot or kernel?My screen also has 1 lane.
Hi !I am designing a SOM board (based on MP2 microprocessor) and I'm wondering if I must take into account the die-to-pin lengths on LPDDR4 IC side. Or does the intrisic architecture of LPDDR4 components garantee internal equivalent lengths ? I didn'...
We have a custom design based on STMP32MP133A na an spi NAND. On paper, using the u-boot diagnostic commands, everything is working correctly.NOTICE: CPU: STM32MP133A Rev.Y NOTICE: Model: Zehnder CCPRO A1R Board INFO: PMIC version = 0x21 INFO: ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.