STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI pinctrl information doesn't show up correctly although SPI bus function properly, is this correct? I expect "AF5" show up instead of "Analog" for pin function.

On my custom board, I configured PZ0, PZ1, PZ2 for SPI1 with device tree, and linux kernel probed successfully and populate spidev node and it works fine, but if look at debug information in /sys/kernel/debug/pinctrl/, it populate something like "pin...

HZhu.12 by Associate II
  • 2079 Views
  • 2 replies
  • 0 kudos

Debian Source list addition

Hi all,I would like to add debian source list to the existing sources in OpenSTLinux.I created a file mysources.list under folder /etc/apt/sources.list and added following lines to itdeb http://ftp.au.debian.org/debian/ buster main contrib non-free d...

NPal.2 by Senior
  • 1703 Views
  • 2 replies
  • 0 kudos

Resolved! Customizing device tree

Help on customizing the device treeI installed my starter package according to instructions at https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_PackageAnd the developer package following instructions at  https://wiki.st.com/stm32m...

MSele.1 by Associate III
  • 3501 Views
  • 6 replies
  • 0 kudos

I get ERROR: Nothing RPROVIDES 'mesa' (but /design/layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-vendorfs.bb RDEPENDS on or otherwise requires it) Error when I try to build core-image-minimal

DISTRO           : <no-custom-config-set>DISTRO_CODENAME  : dunfellMACHINE          : stm32mp1-discoI followed instructions from: https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package#Installing_the_Starter_PackageI initialized repo with:re...

MKaas.1 by Associate III
  • 4956 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.