STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Purpose of external tamper mask, enable interrupt, non-secure masked interrupt status and secure masked interrupt status bits.

Could you explain to me what is the purpose of the different bits associated to the tampers?I am mainly focus on using the passive tampers of the STM32MP1 and I have seen the following configuration bits I don't fully understand:What I understand:Reg...

AGamb.4 by Associate III
  • 2522 Views
  • 3 replies
  • 0 kudos

FDCAN filters not working on STM32mp157

HI,I'm not able to get the FDCAN filter working on a STM32MP157C-DT2. I'm able to receive valid ID' with no problem, however, invalid ID's are getting through.Would someone be kind enough to take a quick look at my setup to make sure I did not miss ...

JSpra by Associate III
  • 3776 Views
  • 2 replies
  • 0 kudos

Could someone help me with some documentation on the configuration of watchpoints in STM32MP157A board?

I was working on the STM32MP157A-DK1 board which has Cortex-A7 + Cortex-M4 processors. I wanted to configure the watchpoints present specifically on the Cortex-A7 processor via C code. The Cortex-A7 technical reference manual indicates the use of MRC...

STM32MP1 Timer

Hi all,I was wondering whether we can achieve a PWM frequence of 1-3Hz with the existing timer which we have. I am targeting to generate a PWM signal within the same frequency range but using A7 as primary.How can we achieve that ?? I do have some id...

NPal.2 by Senior
  • 1423 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to set DDR clock

Hello,I am having a hard time setting the DDR clock at pll2 for an stm32mp157.The clock has been configured to 528MHz using CubeMX. I checked cfg for pll2 in the DeviceTree against the Datasheet / Referance Manual and all settings seem correct.Yet /s...

jvog.sen by Associate II
  • 2953 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.