2022-10-06 5:51 PM
Hi ST Community,
I'm trying to build my linux image for STM32MP157F-EV1 board with the following commands.
Linux Commands:
PC $>cd <working directory path>/Distribution-Package
PC $>mkdir openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15
PC $> cd openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15
PC $>repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15
PC $>repo sync
PC $>DISTRO=openstlinux-weston MACHINE=stm32mp15-eval source layers/meta-st/scripts/envsetup.sh
PC $>bitbake st-image-weston
The following error is outputed and the build stops.
Could you please tell me the cause of the error?
**********************************
ERROR: st-image-resize-initrd-1.0-r0 do_rootfs: Unable to update the package index files. Command '['/home/toku/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Distribution-Package/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-eval/tmp-glibc/work/stm32mp15_eval-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/recipe-sysroot-native/usr/bin/apt-get', 'update']' returned 100:
Solved! Go to Solution.
2022-10-07 8:57 AM
Hello @tatsuya ,
Since you are still using the OpenSTLinux Distribution package v4.0.0, I recommand you to try again with the version v4.0.2 which contains several patchs: https://community.st.com/s/question/0D53W00001lSXndSAG/openstlinux-distribution-patch-release-v402-is-available
You can find it here: https://wiki.st.com/stm32mpu/wiki/STM32_MPU_OpenSTLinux_release_note#Minor_release_updates
---
The error that you have seems similar to this one: https://community.st.com/s/question/0D53W00001njRuoSAE/filesdirectories-were-installed-but-not-shipped-in-any-package
Please take a look at the message that I sent in this community topic, you must be careful to have your distribution package in a folder with a short path.
Hope it helps,
Best Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-10-07 1:55 AM
Hello tatsuya (Community Member)
Any disk space or proxy/access rights issue?
Did you check all the prerequisites first?
https://wiki.st.com/stm32mpu/wiki/PC_prerequisites
Regards,
Olivier
2022-10-07 8:57 AM
Hello @tatsuya ,
Since you are still using the OpenSTLinux Distribution package v4.0.0, I recommand you to try again with the version v4.0.2 which contains several patchs: https://community.st.com/s/question/0D53W00001lSXndSAG/openstlinux-distribution-patch-release-v402-is-available
You can find it here: https://wiki.st.com/stm32mpu/wiki/STM32_MPU_OpenSTLinux_release_note#Minor_release_updates
---
The error that you have seems similar to this one: https://community.st.com/s/question/0D53W00001njRuoSAE/filesdirectories-were-installed-but-not-shipped-in-any-package
Please take a look at the message that I sent in this community topic, you must be careful to have your distribution package in a folder with a short path.
Hope it helps,
Best Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-10-14 12:51 AM
Hi Kevin-san
Thank you for your reply.
My problem was the same as the link below.
It was solved by shortening the path of the directory as below.
/opt/st/DP-MP1-4.0.2
Best regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.