Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.
I am currently developing using the STM32MP157FAD. And I want to create a distribution image and download the image using STM32CubeProgrammer.However, while downloading the image, the following error message is displayed in the log of STM32CubeProgra...
Hi, I have a rather simple question. I use cube mx to generate dts, my Openstlinux is v22.11.23 and during 'bitbake tf-a-stm32mp' I encounter a lack of definition in some '*.c' files like Built stm32image successfully | | CC drivers/st/ddr/s...
I have integrated Micro-ROS into the m4. I have it working such that I am able to publish sensor data and receive it from other nodes. However Micro-ROS takes up a quite a bit of space, 70+ KB. In their documentation it is target at mid tier micro co...
In the recently, for the past few days, I am facing this new issue that, if i compile for my custom som and program, i always get this error. But if I dont do any add-on of packages, I works fine.I even added a simple package like "vim" using IMAGE_I...
HiI'm testing the firmware code using STM32MP157D-DK board.The current configuration for testing use st-link CN11 and ethernet to upload firmware program by using STM32CubeIDE.My question is, Is it possible to do the simmiar firmware program uploadin...
Hello everyone, Currently, I'm using X-CUBE-UCSI and came across some information in the user manual regarding the UCSI Operating Policy Manager (OPM) functionality in STM32MP1 series microprocessors. I was wondering if anyone could point me in the r...
Hi, I am using STM32MP157D-DK1 board to cross compile my application from host pc.My host PC is installed with ubuntu 20.04. I have setup the build environment in host pc. When i am executing the hello exe in STM32MP board.Please find details below. ...
Hi, we tried to send raw ethernet packages using a STM32MP157C-DK2. We used this simple C code here: https://gist.github.com/austinmarton/1922600The code works well on Linux x86 systems as well on Raspbian, but not on the STM32MP157C-DK2 [1]: Sending...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.