2022-02-25 12:29 AM
i am using gst-play-1.0 for testing different bitrate audio play, found that 44.1 kbps, 22.050 kbps were not working but 48kbps mp3 works neatly without noise
Please let me know if i miss anything, i am using I2S1 to derive the base MCLK and feed to codec
log:
gst-play-1.0 /run/media/mmcblk0p1/AudioFiles/test.wav
playing 22.05kbps--- (256*22.05k) = 5644800
Press 'k' to see a list of keyboard shortcuts.
Now playing /run/media/sda1/AudioFiles/BabyElephantWalk60.wav
[ 1164.185749] st,stm32-i2s 44004000.audio-controller: Error -16 setting i2sclk parent clock 5644800
playing 44.1kbps--- (256*44.1k) = 11289600
Now playing /run/media/sda1/AudioFiles/Railroad.mp3
[ 1523.259773] st,stm32-i2s 44004000.audio-controller: Error -16 setting i2sclk parent clock 11289600 -309581440 -309581312
[ 1523.269268] asoc-audio-graph-card sound@0: ASoC: machine hw_params failed: -16
ERROR Could not get/set settings from/on resource. for file:///run/media/sda1/AudioFiles/Railroad.mp3
ERROR debug information: ../../../gst-plugins-base-1.14.4/ext/alsa/gstalsasink.c(617): set_hwparams (): /GstPlayBin:playbin/GstPlaySink:playsink/GstBin:abin/GstBin:bin0/GstAlsaSink:alsasink0:
Unable to set hw params for playback: Device or resource busy
Reached end of play list.
2022-02-25 8:49 AM
Hi any one came across this ?
2022-03-02 3:58 AM
Hi Any body can able to test from eval board ?
2022-03-02 5:17 AM
2022-03-02 5:17 AM
2022-03-03 6:19 AM
Hello @Ara.1 ,
Thank you for the files.
On my side, the two files are working well with the stm32mp157f-dk2 and a headset plugged on the jack plug.
I am using the internal codec with the starter package v3.1.
root@stm32mp1:~# gst-play-1.0 /usr/local/Test_44100.mp3
Press 'k' to see a list of keyboard shortcuts.
Now playing /usr/local/Test_44100.mp3
Redistribute latency...
0:02:00.5 / 0:05:40.9
root@stm32mp1:~# gst-play-1.0 /usr/local/Test_22050.mp3
Press 'k' to see a list of keyboard shortcuts.
Now playing /usr/local/Test_22050.mp3
Redistribute latency...
0:00:05.1 / 0:00:05.1
Reached end of play list.
In your log, you have a lot of error that I didn't have. I think it can explains your errors.
-------------
Which version of ecosystem do you use?
Can I have your DTS file and the complete boot log of your board please?
Regards,
Kevin
2022-03-03 6:59 AM
Hi Kevin,
Thanks for replay
i do see two audio interface
SAI
I2S2
as per board you mentioned,
in command line can you run following command:
root@stm32mp1:~# aplay -l
may you try play gstplay with specific HW or instance where I2S2 runs
root@stm32mp1:~# speaker-test --device hw:0,2 --rate 44100 --channels 2 --format S16_LE --test wav
2022-03-10 9:18 AM
Hello @Ara.1 ,
I am now on a board 157C-DK2 and it works well. Below the results of the two commands that you asked for:
root@stm32mp1:~# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: STM32MP15DK [STM32MP15-DK], device 0: 4400b004.audio-controller-cs42l51-hifi cs42l51-hifi-0 [4400b004.audio-controller-cs42l51-hifi cs42l51-hifi-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
card 0: STM32MP15DK [STM32MP15-DK], device 2: 4000b000.audio-controller-i2s-hifi i2s-hifi-2 [4000b000.audio-controller-i2s-hifi i2s-hifi-2]
Subdevices: 1/1
Subdevice #0: subdevice #0root@stm32mp1:~# speaker-test --device hw:0,2 --rate 44100 --channels 2 --format S16_LE --test wav
speaker-test 1.2.1
Playback device is hw:0,2
Stream parameters are 44100Hz, S16_LE, 2 channels
WAV file(s)
Rate set to 44100Hz (requested 44100Hz)
Buffer size range from 512 to 8192
Period size range from 256 to 4096
Using max buffer size 8192
Periods = 4
was set period_size = 2048
was set buffer_size = 8192
Sample rate doesn't match (48000) for /usr/share/sounds/alsa/Front_Left.wav
root@stm32mp1:~# speaker-test --device hw:0,2 --rate 48000 --channels 2 --format S16_LE --test wav
speaker-test 1.2.1
Playback device is hw:0,2
Stream parameters are 48000Hz, S16_LE, 2 channels
WAV file(s)
Rate set to 48000Hz (requested 48000Hz)
Buffer size range from 512 to 8192
Period size range from 256 to 4096
Using max buffer size 8192
Periods = 4
was set period_size = 2048
was set buffer_size = 8192
0 - Front Left
1 - Front Right
Time per period = 2.863147
0 - Front Left
1 - Front Right-------------------------------------
Please can you answer to these questions:
Please let me know if i miss anything, i am using I2S1 to derive the base MCLK and feed to codecWhich kind of board are you using please? I saw in other topics that you were using a custom board, but is it the case here?
And can you please also send me the traces of the command:
root@stm32mp1:~# aplay -land:
root@stm32mp1:~# pactl list cardsRegards,
Kévin
2022-03-25 9:51 AM
i have the stm32m157C-DK2 board now, i too seen all the bit rates are working, but the mclk is floating , i did a grep on mclk on /sys/debug/clk_summary i do not see any spix_mclk getting created, whic means that i2s2 is slave, and codec is master in the HDMI I2S2,
please correct me if am wrong
2022-04-19 1:18 AM
Hello @Ara.1 ,
As already asked twice I will need your DTS file and your complete DTB to help you.
Can you send me your complete bootlog too please?
I modified my DTS of the DK2 to have the codec CS42L51 as a consumer of SAI2A master clock and it works also.
I would like to have your DTS and DTB as asked above to reproduce a configuration like yours with the i2s2 that feed the codec and reproduce the problem.
In your first log, you had a lot of error i2sclk that looks like error of configuration in the DTS.
Regards,
Kevin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.