2024-11-15 3:07 AM
Hi,
I have a STM32MP157F-DK2 when I try to install something with apt-get I get this error:
root@stm32mp1:~# apt install python3
Reading package lists... Done
Building dependency tree... Done
E: Unable to locate package python3
The date is correct.
If instead I try to run an apt-get update I receive this message:
root@stm32mp1:~# apt-get update
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
Reading package lists... Done
how can i fix it? i need to install python-pip with all dependencies
Best regards
AB
2024-11-15 5:15 AM
Hi @Delios82
please use apt-get install like:
apt-get install python3 python3-pip
Regards
2024-11-15 5:18 AM
2024-11-15 5:37 AM
Perhaps it is really not in the repositories you have configured. At least not the ARM version you would need for the MP1-DK.
This list is usually located in /etc/apt/sources.list .
2024-11-15 7:00 AM
Hi,
I assume your board is correctly connected to network with WLAN or RJ45.
Have you flashed the latest ecosystem ?
example of log
root@stm32mp1:~# apt-get update
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
Get:1 http://packages.openstlinux.st.com/5.1 mickledore InRelease [5723 B]
Get:2 http://packages.openstlinux.st.com/5.1 mickledore/main armhf Packages [705 kB]
Get:3 http://packages.openstlinux.st.com/5.1 mickledore/updates armhf Packages [45.3 kB]
Get:4 http://packages.openstlinux.st.com/5.1 mickledore/untested armhf Packages [1347 kB]
Fetched 2103 kB in 3s (701 kB/s)
Reading package lists... Done
then apt-get install python3 works on my side (tested just now)
Regards.
2024-12-12 1:57 AM
Hi,
I tried to install with the command indicated, I get this error:
root@stm32mp1:~# apt-get install python3-pip
Reading package lists... Done
Building dependency tree
Reading state information... Done
Some packages could not be installed. This may mean that you have
requested an impossible situation or if you are using the unstable
distribution that some required packages have not yet been created
or been moved out of Incoming.
The following information may help to resolve the situation:
The following packages have unmet dependencies:
python3-pip : Depends: python3-unixadmin but it is not going to be installed
E: Unable to correct problems, you have held broken packages.root@stm32mp1:~# apt-get install python3-unixadmin
Reading package lists... Done
Building dependency tree
Reading state information... Done
Some packages could not be installed. This may mean that you have
requested an impossible situation or if you are using the unstable
distribution that some required packages have not yet been created
or been moved out of Incoming.
The following information may help to resolve the situation:
The following packages have unmet dependencies:
python3-unixadmin : Depends: libc6 (>= 2.31+git0+4f0a61f753) but 2.31+git0+2d4f26e5cf-r0.0 is to be installed
Depends: libnsl2 (>= 1.2.0+git0+4a062cf418) but it is not going to be installed
E: Unable to correct problems, you have held broken packages.
root@stm32mp1:~# apt-cache policy python3-pip
python3-pip:
Installed: (none)
Candidate: 20.0.2-r0
Version table:
20.0.2-r0 500
500 http://packages.openstlinux.st.com/3.1 dunfell/main armhf Packages
20.0.2-5ubuntu1.11 500
500 http://ports.ubuntu.com/ubuntu-ports focal-updates/universe armhf Packages
500 http://ports.ubuntu.com/ubuntu-ports focal-security/universe armhf Packages
20.0.2-5ubuntu1 500
500 http://ports.ubuntu.com/ubuntu-ports focal/universe armhf Packages
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.