2019-11-25 2:25 AM
During startup I read the following on the console:
INFO: Loading image id=4 at address 0x2fff0000
INFO: Image id=4 loaded: 0x2fff0000 - 0x30000000
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: STM32 Image size : 801160But those addresses are different than the ones reported into the tsv file:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 tf-a-stm32mp151a-myprj-mx-trusted.stm32
- 0x03 ssbl-boot Binary none 0x0 u-boot-stm32mp151a-myprj-mx-trusted.stm32
P 0x04 fsbl1 Binary mmc0 0x00004400 tf-a-stm32mp151a-myprj-mx-trusted.stm32
P 0x05 fsbl2 Binary mmc0 0x00044400 tf-a-stm32mp151a-myprj-mx-trusted.stm32How they are defined?
How to check they are correct?
Solved! Go to Solution.
2019-11-25 2:57 AM
TSV file define the address where to program the image within the Flash.
The load address in device memory (SYSRAM, DDR) is different and are defined inside each binary image (likely defined at compile time).
2019-11-25 2:57 AM
TSV file define the address where to program the image within the Flash.
The load address in device memory (SYSRAM, DDR) is different and are defined inside each binary image (likely defined at compile time).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.