2024-10-19 4:39 AM
Hi ST Team ,
previously i used the MP1 processor where the video lagging issues, so know i decided to move on another processor who can play the high resolution video above 1080 P @30FPS,
Note: i do not want any HDMI IC's , i want direct pin(RGB) through the processor to our HDMI port,
please suggest me which Processor should be better.
2024-11-21 3:41 AM
But you were using MP157 processor?
If you use this instead to create the rootfs system. This will create a minimum Ubuntu system, which you can use instead of OpenSTLinux. But keep the bootfs.ext4 file.
sudo debootstrap --arch=arm64 noble rootfs http://ports.ubuntu.com/ubuntu-portsThen you "login" to the rootfs system and install Firefox?
sudo chroot rootfs
2024-11-22 2:49 AM - edited 2024-11-22 2:57 AM
@DMårt
Yes previously i used the the MP157 processor but it's so much lagging issues because of the high resolution videos.
on the kirkstone branch i successfully added the chromium browser-x11,
So i decided to move on the MP257, but Krikstone branch is not available on MP2 processor so, i will havet o use another OS.
i am not getting your point "If you use this instead to create the rootfs system. This will create a minimum Ubuntu system, which you can use instead of OpenSTLinux. But keep the bootfs.ext4 file."
how i can use the ubuntu on stm32mp1 processor instead of openstlinux.
do you any reference manual ? , or you used ubuntu OS on stm32mp1 ?
because my hardware team is trying to make custom board of stm32mp2. but currently i hold this project first i need to to implement chromium on stm32mp257f-ev1 then i will make the custom board.
if you have any idea of UBUNTU os on stm32mp157 processor please let me know.
2024-11-22 3:57 AM - edited 2024-11-22 3:58 AM
Try with lower resolution and see if it's helps.
I can teach you how to build an own OS for STM32MP2.
I can create a GitHub repo which you can fork.
I can make a new thread about STM64-OS. That's a good name!
2024-11-22 10:37 PM
@DMårt
I try with lower resolution , but also getting failed
Ya sure it's very helpful for me,
please check the private message i just sent you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.