2020-06-11 5:33 AM
If I build the dts files that come with the developer package, I lose the ethernet. I need to add support for USART3 and UART7, but any new build of the device tree will make the ethernet disappear.
2020-06-11 5:44 AM
Hi @NChri.1
The default dts is exactly the one which is in developer package.
In order to investigate the issue maybe good to look at :
https://wiki.st.com/stm32mpu/wiki/STM32MP15_device_tree
https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration
Olivier
2020-06-11 6:11 AM
Well, I think I followed the wiki
Eventually, I want to edit the file arch/arm/boot/stm157a-dk1.dts (to add those uarts I need to use)
Before modifying it, I built with
make dtbs
and then I copied all the produced dtb files into the boot of the DK2 device. When I do that ethernet is not there anymore.
Note that with the modification of the above file, I do get the uarts, but, as I said, I lose the ethernet (no eth0 found)
I will look into the links you referred to, the second one may be very useful.
Edit: Well, I looked into that... I do not see anything that it is not in my files.
Edit 2: I also lose the wlan...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.