2024-11-21 3:11 AM - edited 2024-11-22 2:53 AM
Hello,
I'm Trying to stream camera over network(ubuntu), using the procedure from STM wiki. But couldn't able to stream.
When I run command in STM32MP135F-DK board, I get the following
root@stm32mp13-disco:~# GST_DEBUG=3 gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw, format=YUY2, width=640, height=480, framerate=30/1 ! encodebin profile="image/jpeg" ! rtpjpegpay
! udpsink host=192.168.23.93 port=5000
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
0:00:00.324857791 4805 0x1e8150 WARN v4l2 gstv4l2object.c:4531:gst_v4l2_object_get_crop_rect:<v4l2src0:src> VIDIOC_CROPCAP failed
0:00:00.353511875 4805 0x1e8150 WARN v4l2 gstv4l2object.c:4531:gst_v4l2_object_get_crop_rect:<v4l2src0:src> VIDIOC_CROPCAP failed
0:00:00.361027041 4805 0x1e8150 WARN v4l2bufferpool gstv4l2bufferpool.c:848:gst_v4l2_buffer_pool_start:<v4l2src0:pool0:src> Uncertain or not enough buffers, enabling copy thresd
0:00:00.981334500 4805 0x1e8118 WARN default gstexiftag.c:1895:gst_tag_list_to_exif_buffer_with_tiff_header: Failed to create exif buffer
Redistribute latency...
0:00:01.111192125 4805 0x1e8118 WARN default gstexiftag.c:1895:gst_tag_list_to_exif_buffer_with_tiff_header: Failed to create exif buffer
0:00:01.241411875 4805 0x1e8118 WARN default gstexiftag.c:1895:gst_tag_list_to_exif_buffer_with_tiff_header: Failed to create exif buffer
0:00:01.370019084 4805 0x1e8118 WARN default gstexiftag.c:1895:gst_tag_list_to_exif_buffer_with_tiff_header: Failed to create exif buffer
0:00:01.497754292 4805 0x1e8118 WARN default gstexiftag.c:1895:gst_tag_list_to_exif_buffer_with_tiff_header: Failed to create exif buffer
0:00:01.623118250 4805 0x1e8118 WARN default gstexiftag.c:1895:gst_tag_list_to_exif_buffer_with_tiff_header: Failed to create exif buffer
0:00:01.753952000 4805 0x1e8118 WARN default gstexiftag.c:1895:gst_tag_list_to_exif_buffer_with_tiff_header: Failed to create exif buffer
0:00:01.874790542 4805 0x1e8118 WARN default gstexiftag.c:1895:gst_tag_list_to_exif_buffer_with_tiff_header: Failed to create exif buffer
0:00:01.995544667 4805 0x1e8118 WARN default gstexiftag.c:1895:gst_tag_list_to_exif_buffer_with_tiff_header: Failed to create exif buffer
0:00:02.116329292 4805 0x1e8118 WARN default gstexiftag.c:1895:gst_tag_list_to_exif_buffer_with_tiff_header: Failed to create exif buffer
0:00:02.237511417 4805 0x1e8118 WARN default gstexiftag.c:1895:gst_tag_list_to_exif_buffer_with_tiff_header: Failed to create exif buffer
And when I run the command in ubuntu, I could get the following
$ gst-launch-1.0 udpsrc port=5000 ! application/x-rtp, encoding-name=JPEG ! rtpjpegdepay ! jpegparse ! decodebin ! videoconvert ! autovideosink
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Got context from element 'autovideosink0': gst.gl.GLDisplay=context, gst.gl.GLDisplay=(GstGLDisplay)"\(GstGLDisplayGBM\)\ gldisplaygbm0";
Setting pipeline to PLAYING ...
New clock: GstSystemClock
And the network connection is established. Checked using the ping command. Can any help me resolve it..?
Thanks,
Ezvan
2024-11-22 1:28 PM
Hi Ezvan
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards
Joe
STMicro Support
2024-11-26 12:00 AM
Hello Joe,
Missed to add a point, When I try to set up the camera subsystem first: I get the below error.
# media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:JPEG_1X8/640x480@1/15 field:none]"
Unable to setup formats: Invalid argument (22)
Thanks,
Ezvan.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.