2020-06-01 7:43 PM
STM32MP1.
Working on an solution that will use OpenAMP between M4 and A7 and then to user space. The M4 will run real time critical code that will send a message to the A7 when data is available, Got the raw and USART samples compiled nder CubeIDE and it''s working as loading the M4 code works.
However wish to use a callback (interrupted) solution in a Linux user space application instead of this user space application polling a device or channel endpoint in a thread to check for data , thus to save CPU load. Even better is avoiding to have to use kernel modules for this A7/M4 brigde. I could not find much use cases of OpenAMP even it's quite an established technology. Any guidance would be helpful.
Solved! Go to Solution.
2020-06-08 7:53 AM
Hi @debugging
>> However how to end the thread when it is in a blocked read and assure graceful exit with all allocated resources in the thread are correctly cleaned up
It exist standard linux solution using SIG (https://man7.org/linux/man-pages/man7/signal.7.html)
>> One idea perhaps is to send a special message to the M4 to let it send a special message to the A7 to terminate
yes it's a solution. Calling VIRT_UART_DeInit on M4 side will destroy endpoint rpmsg, and consequently delete /dev/ttyRPMGx
Olivier
2020-06-03 1:02 AM
Hi @debugging ,
Could details your use case? If I well understood you want to have a Linux userland application that waits for m4 messages but does not consume CPU during this time?
Managing an interrupt callback in the userland is not possible, you have to manage events ( such as udev).
But you probably don’t need to do that. For instance if you have a look to the OpenAMp TTY echo sample, a /dev/ttyRPMSG0 ABI is created.
An application thread reading this file be blocked (until the Cortex-M4 sent a message) without any CPU consumption.
You can do the test by yourself:
Olivier
2020-06-04 8:31 PM
Many thanks. That understanding is correct. The TTY solution should work in in that way if it runs forever. the virtual UART TTY solution runs fine. However how to end the thread when it is in a blocked read and assure graceful exit with all allocated resources in the thread are correctly cleaned up. One idea perhaps is to send a special message to the M4 to let it send a special message to the A7 to terminate . Not sure if there are any other real world solutions so I was looking for something that could be done with the CM4/CA7.
2020-06-08 7:53 AM
Hi @debugging
>> However how to end the thread when it is in a blocked read and assure graceful exit with all allocated resources in the thread are correctly cleaned up
It exist standard linux solution using SIG (https://man7.org/linux/man-pages/man7/signal.7.html)
>> One idea perhaps is to send a special message to the M4 to let it send a special message to the A7 to terminate
yes it's a solution. Calling VIRT_UART_DeInit on M4 side will destroy endpoint rpmsg, and consequently delete /dev/ttyRPMGx
Olivier
2020-06-09 10:40 PM
Thanks, it gets a bit in tricky territory, https://man7.org/linux/man-pages/man7/signal-safety.7.html. the UART option seem the be most safe and clean. The signal may cause to leave the system in unstable state, specially when the main thread needs to continue. Thanks, can close this one.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.