2020-10-29 7:31 AM
Hello,
I am trying to figure out how to drive the USB traffic (any of the available ports acting as device) from/to the M4 core. I can see that the SoC interconnection allows for the data to flow between the peripheral and the M4 core but I cannot find a way to achieve this form of operation.
The runtime operation of the USB-OTG peripheral is assigned to the A7 core but I assume there is a way to allow the endpoint data to be handled by the M4 core in some way (maybe some DMA-based scheme?). I would really appreciate if somebody can cast some light over this issue to get started evaluating this use case.
The target application requires real-time operation for the data being transmitted over USB and this feature being handled by the M4 core is quasi-mandatory. I do not see a clear way of achieving the real-time performance by transmitting all the data over the IPCC interface, even using indirect more, as this would require a very high frequency polling of this memory region by the A7 core.
Thank you very much in advance.
2020-11-05 1:18 AM
Update: I could see several references to the USB-OTG in the CM4 HAL but can still find no driver or support for the peripheral. Is there anything provided by STM I could be missing?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.