STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is there any documentation for configuring UART RX DMA in circular mode properly?

I am trying to configure a DMA stream to capture the RX channel of a UART core on the m4, however, I get very undesirable behaviour.I am trying to set up a circular rx buffer that is of size 10 since the data coming back is of multiples of 5. Unfortu...

STM32 board support eDP bridge?

Hi,We are using stm32mp157c MCU/board and it has DSI output built-in. Now we want to add display port support via DSI to eDP bridge SN65DSI86. It seems that stm32 does not support Displayport output or it has never been done. At least the driver dw_m...

LLe.1 by Associate II
  • 29292 Views
  • 34 replies
  • 0 kudos

Resolved! How can I generate a periodic signal on a GPIO using timer interrupt in Linux kernel (STM32MP153a)?

Hi,I am using STM32MP153a SOC.Linux kernel version is 5.4.56 (openstlinux-5.4-dunfell-mp1-20-11-12).I would like to generate square signal of 50-200 uS on a certain GPIO every 40 ms using Linux kernel.Also ,at this point I need to read certain regist...

vl4ever by Associate
  • 2659 Views
  • 1 replies
  • 0 kudos

Ethernet not working when PHY configured in MII mode in custom board using a STM32MP153CA + automotive Ethernet PHY NXP TJA1101.

I cannot make the Ethernet work on my custom board (STM32MP153CA + automotive Ethernet PHY NXP TJA1101) in U-BOOT (haven't even tried loading kernel). The PHY is connected to an external 25MHz xtal. I'm working with 5-10-dunfell-mp1-21-11-17 files in...

LCast.2 by Associate II
  • 7309 Views
  • 5 replies
  • 0 kudos

Resolved! USB compliance testing

Hi, and yet another question...We would like to perform electrical compliance testing on our USB ports. This requires each port to send a test pattern.Our board has one upstream and two downstream facing ports. The upstream port can be set into vario...

jvog.sen by Associate II
  • 4421 Views
  • 2 replies
  • 0 kudos

Stm32mp157a dac dma issue

Hi,We are using Stm32mp157a processor in my custom board.We are trying to work on dac with DMA but it is not working.You can see my configurations below.In cube mx for DAC there is no Dma option.so we added DMA manually with reference Stm32mp1 Uart ...

DMA2 RX stream5 CM4 not working

Hello , I am trying to configure RX (only) with dma. I am using DMA2 stream5 on usart3 I have connected USB to UART bridge (4 wire) on 40 pin headers RX,TX,VDD(3) and GND on CN7. Whenever I am trying to send any data from the comport (teraterm ) fro...

PVaaz.1 by Associate III
  • 2009 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.