2022-12-12 6:02 PM
While setting up my STM32MP157F-DK2 discovery kit, I followed the steps through the Populate the SDCard section and the flashing process failed with the following message when attempting to flash with the FlashLayout_sdcard_stm32mp157f-dk2-optee.tsv binary.
After failing with the expected flash file I tried flashing again with the FlashLayout_sdcard_stm32mp157c-dk2-optee.tsv binary and the flash process succeeded. Is this expected? I confirmed that my board is a rev F DK-2 and not rev C. I'm not sure what differences there are between the two revisions and if there is any missing functionality with the rev C binary.
16:09:26 : STM32CubeProgrammer API v2.12.0 | Linux-64Bits
16:09:37 : USB speed : High Speed (480MBit/s)
16:09:37 : Manuf. ID : STMicroelectronics
16:09:37 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
16:09:37 : SN : 003F00333438511436383238
16:09:37 : DFU protocol: 1.1
16:09:37 : Board : --
16:09:37 : Device ID : 0x0500
16:10:48 : Read TSV File: /home/loren/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Starter-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/images/stm32mp1/flashlayout_st-image-weston/optee/FlashLayout_sdcard_stm32mp157f-dk2-optee.tsv
16:10:48 : Number of partitions: 13
16:11:45 : Start Embedded Flashing service
16:11:45 : Memory Programming ...
16:11:45 : Opening and parsing file: tf-a-stm32mp157f-dk2-usb.stm32
16:11:45 : File : tf-a-stm32mp157f-dk2-usb.stm32
16:11:45 : Size : 220.38 KB
16:11:45 : Partition ID : 0x01
16:11:45 : Download in Progress:
16:11:46 : File download complete
16:11:46 : Time elapsed during download operation: 00:00:00.902
16:11:46 : RUNNING Program ...
16:11:46 : PartID: :0x01
16:11:46 : Start operation done successfully at partition 0x01
16:11:46 : Memory Programming ...
16:11:46 : Opening and parsing file: fip-stm32mp157f-dk2-optee.bin
16:11:46 : File : fip-stm32mp157f-dk2-optee.bin
16:11:46 : Size : 1.47 MB
16:11:46 : Partition ID : 0x03
16:11:46 : Download in Progress:
16:11:47 : File download complete
16:11:47 : Time elapsed during download operation: 00:00:01.337
16:11:47 : RUNNING Program ...
16:11:47 : PartID: :0x03
16:11:48 : Reconnecting the device ...
16:11:52 : USB speed : High Speed (480MBit/s)
16:11:52 : Manuf. ID : STMicroelectronics
16:11:52 : Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
16:11:52 : SN : 003F00333438511436383238
16:11:52 : DFU protocol: 1.1
16:11:52 : Board : --
16:11:52 : Device ID : 0x0500
16:11:52 : Device name : STM32MP157FAC Rev.Z
16:11:52 : Device type :
16:11:52 : Device CPU :
16:11:52 : Start operation done successfully at partition 0x03
16:11:52 : Flashlayout Programming ...
16:11:52 : Running Flashlayout Partition ...
16:11:52 : Reconnecting the device ...
16:11:52 : USB speed : High Speed (480MBit/s)
16:11:52 : Manuf. ID : STMicroelectronics
16:11:52 : Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
16:11:52 : SN : 003F00333438511436383238
16:11:52 : DFU protocol: 1.1
16:11:52 : Board : --
16:11:52 : Device ID : 0x0500
16:11:52 : Device name : STM32MP157FAC Rev.Z
16:11:52 : Device type :
16:11:52 : Device CPU :
16:11:52 : Flashlayout partition started successfully
16:11:52 : Memory Programming ...
16:11:52 : Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32
16:11:52 : File : tf-a-stm32mp157f-dk2-sdcard.stm32
16:11:52 : Size : 220.41 KB
16:11:52 : Partition ID : 0x04
16:11:52 : Download in Progress:
16:11:53 : File download complete
16:11:53 : Time elapsed during download operation: 00:00:00.122
16:11:53 : RUNNING Program ...
16:11:53 : PartID: :0x04
16:11:53 : Start operation done successfully at partition 0x04
16:11:53 : Memory Programming ...
16:11:53 : Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32
16:11:53 : File : tf-a-stm32mp157f-dk2-sdcard.stm32
16:11:53 : Size : 220.41 KB
16:11:53 : Partition ID : 0x05
16:11:53 : Download in Progress:
16:11:53 : File download complete
16:11:53 : Time elapsed during download operation: 00:00:00.121
16:11:53 : RUNNING Program ...
16:11:53 : PartID: :0x05
16:11:53 : Start operation done successfully at partition 0x05
16:11:53 : Memory Programming ...
16:11:53 : Opening and parsing file: metadata.bin
16:11:53 : File : metadata.bin
16:11:53 : Size : 96.00 B
16:11:53 : Partition ID : 0x06
16:11:53 : Download in Progress:
16:11:53 : File download complete
16:11:53 : Time elapsed during download operation: 00:00:00.006
16:11:53 : RUNNING Program ...
16:11:53 : PartID: :0x06
16:11:53 : Start operation done successfully at partition 0x06
16:11:53 : Memory Programming ...
16:11:53 : Opening and parsing file: metadata.bin
16:11:53 : File : metadata.bin
16:11:53 : Size : 96.00 B
16:11:53 : Partition ID : 0x07
16:11:53 : Download in Progress:
16:11:53 : File download complete
16:11:53 : Time elapsed during download operation: 00:00:00.006
16:11:53 : RUNNING Program ...
16:11:53 : PartID: :0x07
16:11:53 : Start operation done successfully at partition 0x07
16:11:53 : Memory Programming ...
16:11:53 : Opening and parsing file: fip-stm32mp157f-dk2-optee.bin
16:11:53 : File : fip-stm32mp157f-dk2-optee.bin
16:11:53 : Size : 1.47 MB
16:11:53 : Partition ID : 0x08
16:11:53 : Download in Progress:
16:11:54 : File download complete
16:11:54 : Time elapsed during download operation: 00:00:00.788
16:11:54 : RUNNING Program ...
16:11:54 : PartID: :0x08
16:11:54 : Start operation done successfully at partition 0x08
16:11:54 : Memory Programming ...
16:11:54 : Opening and parsing file: st-image-bootfs-openstlinux-weston-stm32mp1.ext4
16:11:54 : File : st-image-bootfs-openstlinux-weston-stm32mp1.ext4
16:11:54 : Size : 64.00 MB
16:11:54 : Partition ID : 0x10
16:11:54 : Download in Progress:
16:11:54 : Error: failed to download Segment[0]
16:11:54 : Error: failed to download the File
16:11:54 : Error: Download partition 0x10 failed
16:11:54 : Error: TSV flashing service failed
16:11:54 : Warning: Connection to device 0x500 is lost
16:11:54 : Disconnected from device.
Solved! Go to Solution.
2022-12-13 2:09 AM
Hello @LGara.1 ,
Sorry, the file available in the post above was for the ecosystem v3.1.
Please can you make a try with this one instead.
Best Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-12-13 1:49 AM
Hello @LGara.1 ,
You encounter the same issue than this post:
https://community.st.com/s/question/0D53W00000wzkIuSAI/fail-the-image-flashing-on-stm32mpu157fdk2
Please can you make a try with the file shared in Best Answer.
Best Regards,
Kevin
2022-12-13 2:09 AM
Hello @LGara.1 ,
Sorry, the file available in the post above was for the ecosystem v3.1.
Please can you make a try with this one instead.
Best Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-12-13 6:23 PM
Thanks! This resolved the issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.