2020-08-25 5:17 AM
Hello.
I'm trying to connect MP1's eth to Marvell 88E6352. Switch connected to cpu via RGMII.
Because switch don't have output 125MHZ clock, eth configured to use internal clock, how described in this article: https://community.st.com/s/question/0D50X0000B8iBSB/stm32mp157-ethernet-problem
After all connections and configurations Linux can see Marvell's switch. But when I try to enable eth, it's not started and write this to console:
root@stm32mp1:~# ifconfig eth0 up
[ 107.460160] Generic PHY fixed-0:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=fixed-0:00, irq=POLL)
[ 108.476843] stm32-dwmac 5800a000.ethernet: Failed to reset the dma
[ 108.481623] stm32-dwmac 5800a000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[ 108.490893] stm32-dwmac 5800a000.ethernet eth0: stmmac_open: Hw setup failed
ifconfig: SIOCSIFFLAGS: Device or resource busyI can't solve this problem by myself.
2020-09-30 12:38 AM
Hi @Community memberomissarov ,
Could you please share the following informations to progress on the analysis :
Thanks,
BR,
Christophe
2020-10-01 10:59 AM
Hi Christophe,
Thank you for answering.
As base for my firmware I use Yocto_Install1-1 (version: 1.1.0) from there:
dts files for u-boot and kernel in attach, also with dmesg and clk_summary dumps.
WBR, Dmitry
2020-10-01 11:48 PM
Hi,
for HW point of view, this kind of error is usually shown because the ETH GMAC IP does not receive rx and tx clock. looking at Reference Manual figure "Peripheral clock distribution for Ethernet" might help to see which settings are needed. This wiki article and AN5031 could also help.
2020-10-02 1:32 AM
Hello, @PatrickF
My clk_summary contains next values:
ref3 1 1 0 24000000 0 0 50000
pll3 2 2 0 624999609 0 0 50000
pll3_r 0 0 0 11160708 0 0 50000
pll3_q 1 1 0 124999922 0 0 50000
ethptp_k 0 0 0 124999922 0 0 50000
ethck_k 1 1 0 124999922 0 0 50000
...
ref1 2 2 0 24000000 0 0 50000
pll2 2 2 0 533000000 0 0 50000
pll2_r 1 1 0 533000000 0 0 50000
pll2_q 0 0 0 533000000 0 0 50000
gpu_k 0 0 0 533000000 0 0 50000
pll2_p 1 1 0 266500000 0 0 50000
ck_axi 8 9 0 266500000 0 0 50000
...
ethstp 0 0 0 266500000 0 0 50000
...
ethmac 1 1 0 266500000 0 0 50000
ethrx 1 1 0 266500000 0 0 50000
ethtx 1 1 0 266500000 0 0 50000
...As I can understand, ETH have rx and tx clocks. Or I'm wrong?
2020-10-05 5:51 AM
As I'm HW guy, I cannot rely/check if SW log is ok.
Apart 125MHz settings, to be sure, you could check directly low level registers setting (mostly SYSCFG and RCC) according to your expectations regarding "Peripheral clock distribution for Ethernet" clock paths.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.