2024-02-07 3:39 AM - edited 2024-02-07 3:43 AM
Hi there,
During OP-TEE integration of our custom platform based on STM32MP151C MPU I'm facing an issue with DFU. It looks like the dfu command stucks in `run_usb_dnl_gadget` inside the loop and waits forever for the flush flag:
NOTICE: CPU: STM32MP151CAC Rev.Z
NOTICE: Model: STMicroelectronics custom STM32CubeMX board (TF-A)
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.6-stm32mp1-r1.0(debug):v2.6-dirty
NOTICE: BL2: Built : 13:14:26, Nov 23 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
INFO: Memory size = 0x8000000 (128 MB)
INFO: DFU USB START...
INFO: phase ID :3, Manifestation 3 at c7159862
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 31
INFO: Loading image id=31 at address 0x2ffff000
INFO: Image id=31 loaded: 0x2ffff000 - 0x2ffff1fa
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc0000
INFO: Image id=4 loaded: 0x2ffc0000 - 0x2ffc002c
INFO: OPTEE ep=0x2ffc0000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x2
INFO: BL2: Loading image id 21
INFO: Loading image id=21 at address 0x2ffc0000
INFO: Image id=21 loaded: 0x2ffc0000 - 0x2ffda710
INFO: BL2: Loading image id 22
INFO: Loading image id=22 at address 0xc6200000
INFO: Image id=22 loaded: 0xc6200000 - 0xc6254000
INFO: BL2: Loading image id 23
INFO: Loading image id=23 at address 0xc0500000
INFO: Image id=23 loaded: 0xc0500000 - 0xc0511fb0
INFO: BL2: Skip loading image id 26
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc01d8e54
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffc0000
INFO: SPSR = 0x1d3
I/TC: Early console on UART#4
I/TC:
I/TC: Pager is enabled. Hashes: 2784 bytes
I/TC: Pager pool size: 60kB
I/TC: Non-secure external DT found
I/TC: Embedded DTB found
I/TC: OP-TEE version: 3.16.0-dev (gcc version 12.2.0 (GCC)) #24 Fri Jan 28 02:28:18 PM UTC 2022 arm
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: DT clock tree configurations were ignored
I/TC: WARNING: All debug access are allowed
I/TC: Platform stm32mp1: flavor PLATFORM_FLAVOR - DT stm32mp151c-0068-new-1-mx.dts
I/TC: DTB enables console (non-secure)
I/TC: Primary CPU switching to normal world boot
U-Boot 2021.10-stm32mp-r1-dirty (Oct 04 2021 - 15:09:26 +0000)
U-Boot code: C0100000 -> C01C0BF4 BSS: -> C01CD568
psci psci: set_state_simple op missing
stm32mp_bsec efuse@5c005000: set_state_simple op missing
CPU: STM32MP151CAC Rev.Z
Model: STMicroelectronics custom STM32CubeMX (U-Boot)
Board: stm32mp1 in trusted mode (st,stm32mp151c-0068-new-linux-mx)
DRAM: stm32mp1_ddr ddr@5a003000: set_state_simple op missing
Monitor len: 000CD568
Ram size: 08000000
Ram top: C6200000
Reserving 821k for U-Boot at: c6122000
Reserving 33024k for malloc() at: c40e2000
Reserving 1M for noncached_alloc() at: c3f00000
Reserving 72 Bytes for Board Info at: c3efffb0
Reserving 216 Bytes for Global Data at: c3effed0
Reserving 72640 Bytes for FDT at: c3eee310
RAM Configuration:
Bank #0: c0000000
DRAM: 128 MiB
New Stack Pointer is: c3eee2f0
Relocation Offset is: 06022000
Relocating to c6122000, new gd at c3effed0, sp at c3eee2f0
Clocks:
- MPU : 650 MHz
- MCU : 200 MHz
- AXI : 266.500 MHz
- PER : 0 MHz
- DDR : 533 MHz
WDT: Started with servicing (32s timeout)
NAND: 0 MiB
MMC: pinconfig sdmmc2_mx-0: set_state_simple op missing
STM32 SD/MMC: 1, STM32 SD/MMC: 0
Loading Environment from nowhere... OK
In: serial@40010000
Out: serial@40010000
Err: serial@40010000
Net: Ethernet disabled.
Hit any key to stop autoboot: 0
Boot over usb0!
stm32prog_is_stm32_header_v1:invalid magic number : 0x55555555
stm32prog_is_stm32_header_v2:invalid magic number : 0x55555555
stm32prog_is_stm32_header_v1:invalid magic number : 0x55555555
stm32prog_is_stm32_header_v2:invalid magic number : 0x55555555
DFU alt info setting: dfu_alt_add(ram, NULL,@FlashLayout/0x00/1*256Ke) result 0
dfu_alt_add(virt,241,@virtual/0xf1/1*512Be) result 0
optee_ta result 0
dfu_alt_add(virt,242,@OTP/0xf2/1*776Be) result 0
dfu_alt_add(virt,244,@PMIC/0xf4/1*8Be) result 0
done
dwc2-udc-otg usb-otg@49000000: set_state_simple op missing
stm32mp1_clk rcc@50000000: stm32mp1_clk_enable: id clock 166 has been enabled
stm32_rcc_reset rcc@50000000: reset id = 19656 bank = 2456 offset = 8)
stm32_rcc_reset rcc@50000000: reset id = 19656 bank = 2456 offset = 8)
registering UDC driver [<NULL>]
==== PP: run_usb_dnl_gadget:42
I also observed that `ID 0483:df11 STMicroelectronics STM Device in DFU Mode` USB device is missing on my host at that state.
The same configuration works well without OP-TEE and STM32_Programmer_CLI successfully uploads the images. I don't see any relation between OP-TEE and stm32prog/DFU, but looks like something is wrong or missing.
I use the stm32mpu-ecosystem-v4 provided by the meta-st-stm32mp yocto layer (langdale).
I would be grateful for any hints or places that should be checked in such a case.
Thanks in advance
Solved! Go to Solution.
2024-02-21 2:43 AM
The missing part that makes it work is an assignment of the correct phys and phy-supply properties to the u-boot's DTS as follows:
&usbotg_hs{
u-boot,dm-pre-reloc;
status = "okay";
phys = <&usbphyc_port1 0>;
};
&usbphyc_port0{
u-boot,dm-pre-reloc;
status = "okay";
phy-supply = <&fixed_3v3>;
};
&usbphyc_port1{
u-boot,dm-pre-reloc;
status = "okay";
phy-supply = <&fixed_3v3>;
};
2024-02-08 6:06 AM
I/TC: DT clock tree configurations were ignored
2024-02-12 1:26 AM
This property doesn't change anything in my case.
@PatrickD wrote:can you check that you have in U-Boot device tree addon&usbotg_hs {u-boot,force-b-session-valid;};
The output of above commands looks exactly the same as in the working setup without OP-TEE integrated. I also found out that in the OP-TEE variant there is no possibility to enable the usb33 regulator:Or Clr^C in U-Boot console to stop stm32prog command andthen you can use U-Boot commands to debug the issuefor example:> regulator status -a> clk dump
> dm tree
STM32MP> regulator dev usb33
dev: usb33 @ usb33
STM32MP> regulator enable
stm32mp_pwr_regulator usb33: Turning on usb33
D/TC:0 pwr_scv_handler:54 PWR service: write 0x1000000 at offset 0xc
stm32mp_pwr_regulator usb33: usb33: timeout
Regulator: usb33 - can't enable!
Error: -110 (Connection timed out)
If RCC is not secured (see TZEN / MCKPROT) and if the PMIC is not managed in OP-TEE.Today it is not the case for STMicroelectronics boards on STM32MP15, I assumed it inot the case for your port if you aligned your board with our boards.
D/TC:0 0 check_rcc_secure_configuration:506 RCC/PWR secure hardening: TZEN enable, MCKPROT enable
So, if I understand correctly, according to my TZEN/MCKPROT settings, there is a need to do the same as it is declared in u-boot's arch/arm/dts/stm32mp131.dtsi:But is if the RCC/PWR/OP-TEE are securized, the associated ressource are no more accessible,and the associated regulator must be exported by as it is done SCMI STM32MP13:usbotg_hs: usb-otg@49000000 {compatible = "st,stm32mp15-hsotg", "snps,dwc2";......usb33d-supply = <&usb33>; => MP15usb33d-supply = <&scmi_usb33>; => MP13.....status = "disabled";};
firmware {
// ...
scmi: scmi {
// ...
scmi_voltd: protocol@17 {
reg = <0x17>;
scmi_regu: regulators {
// ..
scmi_usb33: voltd-usb33 {
voltd-name = "usb33";
regulator-name = "usb33";
};
};
};
};
};
A strange line in the traceI/TC: DT clock tree configurations were ignoredIf the clock tree is not coorectly applied in OP-TEE, that explain some USB issue....
You can compare the clock tree in OP-TEE with ST boards.
/*
* OP-TEE core is not in charge of configuring clock parenthood.
* This is expected from an earlier boot stage. Modifying the clock
* tree parenthood here may jeopardize already configured clocks.
* The sequence below ignores such DT directives with a friendly
* debug trace.
*/2024-02-21 2:43 AM
The missing part that makes it work is an assignment of the correct phys and phy-supply properties to the u-boot's DTS as follows:
&usbotg_hs{
u-boot,dm-pre-reloc;
status = "okay";
phys = <&usbphyc_port1 0>;
};
&usbphyc_port0{
u-boot,dm-pre-reloc;
status = "okay";
phy-supply = <&fixed_3v3>;
};
&usbphyc_port1{
u-boot,dm-pre-reloc;
status = "okay";
phy-supply = <&fixed_3v3>;
};
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.