2022-06-13 4:40 AM
Hi,
We are using stm32mp157a in our custom board.We are configured SAI for Cortex M in cubemx.But we are unable to get dma interrupt and data through DMA. you can see my code flow below.
In main.
we are calling below functions.
int main()
{
MX_DMA_Init();
MX_SAI2_Init();
HAL_SAI_Receive_DMA(&hsai_BlockB2,(uint8_t *)AUDIORecvBuf,BUF_SIZE);
while(1)
{
}
}
1.SAI intialization
static void MX_SAI2_Init(void)
{
/* USER CODE BEGIN SAI2_Init 0 */
/* USER CODE END SAI2_Init 0 */
/* USER CODE BEGIN SAI2_Init 1 */
/* USER CODE END SAI2_Init 1 */
hsai_BlockA2.Instance = SAI2_Block_A;
hsai_BlockA2.Init.Protocol = SAI_FREE_PROTOCOL;
hsai_BlockA2.Init.AudioMode = SAI_MODESLAVE_RX;
hsai_BlockA2.Init.DataSize = SAI_DATASIZE_16;
hsai_BlockA2.Init.FirstBit = SAI_FIRSTBIT_MSB;
hsai_BlockA2.Init.ClockStrobing = SAI_CLOCKSTROBING_FALLINGEDGE;
hsai_BlockA2.Init.Synchro = SAI_ASYNCHRONOUS;
hsai_BlockA2.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE;
hsai_BlockA2.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_HF;
hsai_BlockA2.Init.MckOutput = SAI_MCK_OUTPUT_ENABLE;
hsai_BlockA2.Init.SynchroExt = SAI_SYNCEXT_DISABLE;
hsai_BlockA2.Init.MonoStereoMode = SAI_STEREOMODE;
hsai_BlockA2.Init.CompandingMode = SAI_NOCOMPANDING;
hsai_BlockA2.Init.TriState = SAI_OUTPUT_NOTRELEASED;
hsai_BlockA2.Init.PdmInit.Activation = DISABLE;
hsai_BlockA2.Init.PdmInit.MicPairsNbr = 0;
hsai_BlockA2.Init.PdmInit.ClockEnable = SAI_PDM_CLOCK1_ENABLE;
hsai_BlockA2.FrameInit.FrameLength = 64;
hsai_BlockA2.FrameInit.ActiveFrameLength = 1;
hsai_BlockA2.FrameInit.FSDefinition = SAI_FS_STARTFRAME;
hsai_BlockA2.FrameInit.FSPolarity = SAI_FS_ACTIVE_HIGH;
hsai_BlockA2.FrameInit.FSOffset = SAI_FS_FIRSTBIT;
hsai_BlockA2.SlotInit.FirstBitOffset = 0;
hsai_BlockA2.SlotInit.SlotSize = SAI_SLOTSIZE_DATASIZE;
hsai_BlockA2.SlotInit.SlotNumber = 4;
hsai_BlockA2.SlotInit.SlotActive = 0x0000000F;
if (HAL_SAI_Init(&hsai_BlockA2) != HAL_OK)
{
Error_Handler();
}
hsai_BlockB2.Instance = SAI2_Block_B;
hsai_BlockB2.Init.Protocol = SAI_FREE_PROTOCOL;
hsai_BlockB2.Init.AudioMode = SAI_MODESLAVE_TX;
hsai_BlockB2.Init.DataSize = SAI_DATASIZE_16;
hsai_BlockB2.Init.FirstBit = SAI_FIRSTBIT_MSB;
hsai_BlockB2.Init.ClockStrobing = SAI_CLOCKSTROBING_FALLINGEDGE;
hsai_BlockB2.Init.Synchro = SAI_SYNCHRONOUS;
hsai_BlockB2.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE;
hsai_BlockB2.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_HF;
hsai_BlockB2.Init.MckOutput = SAI_MCK_OUTPUT_ENABLE;
hsai_BlockB2.Init.SynchroExt = SAI_SYNCEXT_DISABLE;
hsai_BlockB2.Init.MonoStereoMode = SAI_STEREOMODE;
hsai_BlockB2.Init.CompandingMode = SAI_NOCOMPANDING;
hsai_BlockB2.Init.TriState = SAI_OUTPUT_NOTRELEASED;
hsai_BlockB2.Init.PdmInit.Activation = DISABLE;
hsai_BlockB2.Init.PdmInit.MicPairsNbr = 0;
hsai_BlockB2.Init.PdmInit.ClockEnable = SAI_PDM_CLOCK1_ENABLE;
hsai_BlockB2.FrameInit.FrameLength = 64;
hsai_BlockB2.FrameInit.ActiveFrameLength = 1;
hsai_BlockB2.FrameInit.FSDefinition = SAI_FS_STARTFRAME;
hsai_BlockB2.FrameInit.FSPolarity = SAI_FS_ACTIVE_HIGH;
hsai_BlockB2.FrameInit.FSOffset = SAI_FS_FIRSTBIT;
hsai_BlockB2.SlotInit.FirstBitOffset = 0;
hsai_BlockB2.SlotInit.SlotSize = SAI_SLOTSIZE_DATASIZE;
hsai_BlockB2.SlotInit.SlotNumber = 4;
hsai_BlockB2.SlotInit.SlotActive = 0x0000000F;
if (HAL_SAI_Init(&hsai_BlockB2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SAI2_Init 2 */
/* USER CODE END SAI2_Init 2 */
}
2.SAI DMA Configuration.
i)sai2_A :
hdma_sai2_a.Instance = DMA2_Stream0;
hdma_sai2_a.Init.Request = DMA_REQUEST_SAI2_A;
hdma_sai2_a.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_sai2_a.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_sai2_a.Init.MemInc = DMA_MINC_ENABLE;
hdma_sai2_a.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_sai2_a.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
hdma_sai2_a.Init.Mode = DMA_CIRCULAR;
hdma_sai2_a.Init.Priority = DMA_PRIORITY_VERY_HIGH;
hdma_sai2_a.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
hdma_sai2_a.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_sai2_a.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_sai2_a.Init.PeriphBurst = DMA_PBURST_SINGLE;
if (HAL_DMA_Init(&hdma_sai2_a) != HAL_OK)
{
Error_Handler();
}
/* Several peripheral DMA handle pointers point to the same DMA handle.
Be aware that there is only one channel to perform all the requested DMAs. */
__HAL_LINKDMA(hsai,hdmarx,hdma_sai2_a);
__HAL_LINKDMA(hsai,hdmatx,hdma_sai2_a);
ii)SAI2_B:
hdma_sai2_b.Instance = DMA2_Stream1;
hdma_sai2_b.Init.Request = DMA_REQUEST_SAI2_B;
hdma_sai2_b.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_sai2_b.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_sai2_b.Init.MemInc = DMA_MINC_ENABLE;
hdma_sai2_b.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_sai2_b.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
hdma_sai2_b.Init.Mode = DMA_NORMAL;
hdma_sai2_b.Init.Priority = DMA_PRIORITY_HIGH;
hdma_sai2_b.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
hdma_sai2_b.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_HALFFULL;
hdma_sai2_b.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_sai2_b.Init.PeriphBurst = DMA_PBURST_SINGLE;
if (HAL_DMA_Init(&hdma_sai2_b) != HAL_OK)
{
Error_Handler();
}
/* Several peripheral DMA handle pointers point to the same DMA handle.
Be aware that there is only one channel to perform all the requested DMAs. */
__HAL_LINKDMA(hsai,hdmarx,hdma_sai2_b);
__HAL_LINKDMA(hsai,hdmatx,hdma_sai2_b);
3.DMA intialization
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMAMUX_CLK_ENABLE();
__HAL_RCC_DMA2_CLK_ENABLE();
/* DMA interrupt init */
/* DMA2_Stream0_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn);
/* DMA2_Stream1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream1_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream1_IRQn);
}
How can i resolve this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.