2022-02-28 3:21 PM
Hi!
I ordered now a STM32H747I-DISCO board. Have looked in the source tree from U-Boot (ST fork and mainline). I know there is a support for STM32H743I-EVAL board. Wondering why there isn't a support for the STM32H747I-DISCO.
Generic question:
Has somebody interests when I add U-Boot support for the STM32H747I-DISCO Board?
(Maybe I could also add Linux support. Okay, 32MiB is maybe not enough RAM...)
It's maybe only a gimmick...
2022-02-28 3:43 PM
>>Has somebody interests when I add U-Boot support for the STM32H747I-DISCO Board?
Relatively low I'd suspect. The ability to pull data via Ethernet and into internal/external flash has some appeal, but uBoot and ucLinux have minimal traction.
>>Maybe I could also add Linux support.
With so many better embedded linux platforms, one wonders why?
2022-02-28 4:00 PM
>>With so many better embedded linux platforms, one wonders why?
That's true. But there was also support for the STM32H743I-EVAL board in Linux.
U-Boot:
I have also released patches for none-STMicroelectronics platforms (device driver as example) for U-Boot. But currently don't add a specific board. It's for the purpose of education and a fun project for me.
Why I use STM32 platforms?
I want to develop a RT micro kernel and because the STM32 products are really good documented, I choose this as starting platform...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.