2021-09-28 12:23 AM
I've enabled pps-gpio and pps in the kernel config and added the following to the device tree:
/{
//...
pps{
compatible = "pps-gpio";
gpios = <&gpiod 13 GPIO_PULL_UP>;
status = "okay";
};
};but this results in the following when starting the system:
[ 1.350093] pps-gpio pps: failed to request PPS GPIO
[ 1.350132] pps-gpio: probe of pps failed with error -22do you have any hint for me how i can fix that?
I also tried adding a pinctrl section (which resulted in other problems).
Thanks!
Thomas
Solved! Go to Solution.
2021-10-05 6:25 AM
Hi Thomas,
Indeed, documentation is clear on the DT syntax and is apparently not deprecated. So I used the same DT node you used with same pins (exactly as you did), updated the linux menuconfig to enable all the pps options, recompiled the kernel and tested on a STM32MP157C-DK2 board.
did an update of the modules (depmod -a, sync). Everything looks fine.
root@stm32mp1:~# dmesg | grep pps
[ 0.145980] pps_core: LinuxPPS API ver. 1 registered
[ 0.145998] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giom>
[ 12.644460] pps_core: source pps.-1 got cdev (251:0)
[ 12.644496] pps pps0: new PPS source pps.-1
[ 12.647391] pps pps0: Registered IRQ 88 as PPS source
root@stm32mp1:~# lsmod | grep pps
pps_gpio 16384 0
root@stm32mp1:~# cat /proc/interrupts | grep pps
88: 0 0 stm32gpio 13 Edge pps.-1
Regards,
Olivier
2021-09-29 9:21 AM
Hello thomas987 (Community Member)
PB5 ou PG8 are the pins for the pps-out signals. Why do you use PD13?
Regards,
Olivier
2021-09-30 2:25 AM
Hi,
the pps-gpio module is used for pps input -- to measure and timestamp an incoming PPS signal. It actually should work with any GPIO pin but it always fails here:
https://github.com/STMicroelectronics/linux/blob/v5.10-stm32mp/drivers/pps/clients/pps-gpio.c#L110
at the devm_gpiod_get call.
Best Regards
Thomas
2021-09-30 9:50 AM
Hi Thomas,
ok I understand now.
data->gpio_pin = devm_gpiod_get(&pdev->dev, NULL, GPIOD_IN);
instead of "NULL" I would expect "pps" instead. (parsing the DT for pps-gpios then extract the gpio pin).
I will check this point.
Best Regards,
Olivier
2021-10-01 2:04 AM
Hi Oliver,
> instead of "NULL" I would expect "pps" instead. (parsing the DT for pps-gpios then extract the gpio pin).
the second parameter should only specify the name used for the gpio handle, right? so "pps" would look for "pps-gpios" and NULL should look for "gpios" in the device tree like I specified: `gpios = <&gpiod 13 GPIO_PULL_UP>;`.
> I will check this point.
Thanks!
Best Regards,
Thomas
2021-10-05 6:25 AM
Hi Thomas,
Indeed, documentation is clear on the DT syntax and is apparently not deprecated. So I used the same DT node you used with same pins (exactly as you did), updated the linux menuconfig to enable all the pps options, recompiled the kernel and tested on a STM32MP157C-DK2 board.
did an update of the modules (depmod -a, sync). Everything looks fine.
root@stm32mp1:~# dmesg | grep pps
[ 0.145980] pps_core: LinuxPPS API ver. 1 registered
[ 0.145998] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giom>
[ 12.644460] pps_core: source pps.-1 got cdev (251:0)
[ 12.644496] pps pps0: new PPS source pps.-1
[ 12.647391] pps pps0: Registered IRQ 88 as PPS source
root@stm32mp1:~# lsmod | grep pps
pps_gpio 16384 0
root@stm32mp1:~# cat /proc/interrupts | grep pps
88: 0 0 stm32gpio 13 Edge pps.-1
Regards,
Olivier
2021-10-07 1:13 AM
Hi,
thanks for checking!
Yes, indeed, it seems to work now as a kernel module (=m) but fails when i build it into the kernel (=y)
Best Regards and thanks for your help!
Thomas
2022-01-25 9:17 PM
I have a same problem. The reason is that GPIO controller probes later then PPS. Initialization order is correct, but platrofm_devices are probed in different order. I fixed order by adding
pinctrl-names = "default";
pinctrl-0 = <&pinctrl>;in y pps node. Note that if you using piz, you should set &pinctrl_z instead of &pinctrl.
I'm not sure is it solution or workaround, because I seen another configuration in iMX devicetree examples:
pps {
pinctrl-names = "default";
pinctrl-0 = <&pps_pins>;
gpios = <&gpioi 10 GPIO_ACTIVE_HIGH>;
compatible = "pps-gpio";
status = "okay";
};
&pinctrl {
pps_pins: pps_pins-0 {
pins {
pinmux = <STM32_PINMUX('I', 10, GPIO)>;
};
};
};
But in this case devm_gpiod_get in PPS driver says that this GPIO pin already requested by PPS driver (and after reading the sysfs I was convinced that this was the case ), and I don't know how I can get the gpio descriptor already requested in the driver.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.