2020-08-11 8:33 AM
Hi, I try upload Openstlinux-5.4-dunfell-mp1-20-06-24 in a stm32mp157c-ev1(Nand).
I used STM32_Programmer_CLI version 2.3.0 and I get the next error:
------------------------STM32_Programmer_CLI ---------------------------------
reconnecting the device ...
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2000, @Name /STM32MP157CAA Rev.B,
SN : 0026003D3338510439303435
FW version : 0x0110
Device ID : unknown
Start operation done successfully at partition 0x03
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157c-ev1-trusted.stm32
File : tf-a-stm32mp157c-ev1-trusted.stm32
Size : 241984 Bytes
Partition ID : 0x04
Download in Progress:
Error: failed to download Segment[0]
Error: failed to download the File
Time elapsed during download operation: 00:00:30.005
Error: Download partition 0x04 failed
Error: TSV flashing service failed
-------------------------------------------------------------------------------
-----------------------U-Boot 2020.01-stm32mp-r1 (Board)--------------
U-Boot 2020.01-stm32mp-r1 (Jan 06 2020 - 20:56:31 +0000)
CPU: STM32MP157CAA Rev.B
Model: STMicroelectronics STM32MP157C eval daughter on eval mother
Board: stm32mp1 in trusted mode (st,stm32mp157c-ev1)
Board: MB1263 Var1.0 Rev.C-02
DRAM: 1 GiB
Clocks:
- MPU : 650 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
WDT: Started with servicing (32s timeout)
NAND: 1024 MiB
MMC: STM32 SD/MMC: 0, STM32 SD/MMC: 1
In: serial
Out: serial
Err: serial
Net: eth0: ethernet@5800a000
Hit any key to stop autoboot: 0
Boot over usb0!
partitions : done
DFU alt info setting: using id 'nand0,0'
using id 'nand0,1'
using id 'nand0,2'
using id 'nand0,3'
done
#
UPLOAD ... done
Ctrl+C to exit ...
dfu_write: Wrong sequence number! [0] [2]
------------------------------------------------------------------------------------
With the last release of STM32CubeProgrammer (2.5.0) work and i can upload the Demo.
I would like to know why STM32CubeProgrammer (2.3.0) is not compatible with Openstlinux-5.4-dunfell-mp1-20-06-24. I see changelog of openstlinux and i don't find nothing about it.
Thanks!!
Solved! Go to Solution.
2020-09-10 2:50 PM
For information,
in U-Boot for V2.0, "@Name" with full SOC name is provide during USB enumeration:
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2000, @Name /STM32MP157CAA Rev.B,
but this field is compatible only with the latest ST32CubePRogrammer version (> 2.4.0)
FYI v2.5.0 is indicated in STM32MP15-ecosystem-v2.0.0 release = https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note
else the ID is not detected and load failed, it is indicated in the trace by:
...
Device ID : unknown
....
Patrick
2020-08-11 9:30 AM
Probably because Openstlinux-5.4-dunfell-mp1-20-06-24 was released after v2.3.0 and the software is not forwards compatible.
Just a guess.
2020-08-11 2:09 PM
Hi, TDK. Thanks for aswer.
Yes, Openstlinux-5.4-dunfell-mp1-20-06-24 was released after v2.3.0 but v2.4.0 also and with v2.4.0 work fine.
I guess the problem comes from the u-boot but I'd like to know that it's changed.
2020-09-10 2:50 PM
For information,
in U-Boot for V2.0, "@Name" with full SOC name is provide during USB enumeration:
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2000, @Name /STM32MP157CAA Rev.B,
but this field is compatible only with the latest ST32CubePRogrammer version (> 2.4.0)
FYI v2.5.0 is indicated in STM32MP15-ecosystem-v2.0.0 release = https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note
else the ID is not detected and load failed, it is indicated in the trace by:
...
Device ID : unknown
....
Patrick
2020-09-16 12:03 AM
Hi, Patrick!
That's all I needed to know.
Thanks you!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.