2024-08-07 4:03 PM - edited 2024-08-07 4:07 PM
It's fun to debugging the output when I flashing the processor/eMMC from CubeProgrammer via USB. But it's less fun to not knowing the cause of the error.
What can it be in this case?
Do I have forgot the sett the board ID, is the unknown VDD the error?
What I have done, is to copy the most of stm32mp15xx-dk1.dtsi into stm32mp15x-<your project device tree>-mx.dts because my custom made bord is the same as STM32MP157D-DK1 + eMMC boot.
See the post here: Debug Output UART
My device tree .dts files: Device Tree STM32MP151AAC3
2024-08-08 2:28 AM
Hello @DMårt ,
Sorry but I cannot access your logs, can you put it here ?
Concerning the log you put in title, this is not an error log. It just says that the number of Failed probed item is 0.
I will need the info of your first link to go deeper.
Can you also precise me your software version ?
Kind regards,
Erwan.
2024-08-08 3:37 AM
Hello @Erwan SZYMANSKI
I upload the log here as a text file: https://easyupload.io/ykdhui
Yes. I can give you the whole software: https://github.com/DanielMartensson/STM32-Computer/tree/main/Firmware/STM32-Computer-Firmware
I'm running CubeIDE 1.16.0 version with latest SDK and Sources.
2024-08-08 4:49 AM
@DMårt ,
I see PMIC configuration under I2C4 node in your TF-A DTS and no PMIC configuration in OP-TEE device tree. Moreover I see TF-A logs showing PMIC version so I guess your PCB is not power discrete. Please align the different information between your component device trees.
Kind regards,
Erwan.
2024-08-08 10:49 AM
Hello @Erwan SZYMANSKI
Yes. By adding the PMIC for the Op-Tee, I get a different result.
"assertion 'info.reg != DT_INFO_INVALID_REG && info.reg_size != DT_INFO_INVALID_REG_SIZE' failed at core/drivers/stm32_uart.c:156 <stm32_uart_init_from_dt_node>" - What does this mean?
I/TC: OP-TEE version: 8e92eeff0-dev (gcc version 12.3.0 (GCC)) #9 Thu Aug 8 17:16:17 UTC 2024 arm
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
D/TC:0 0 call_preinitcalls:21 level 2 mobj_mapped_shm_init()
D/TC:0 0 mobj_mapped_shm_init:463 Shared memory address range: dbc00000, ddc00000
D/TC:0 0 call_initcalls:40 level 1 register_time_source()
D/TC:0 0 call_initcalls:40 level 1 initialize_bsec()
D/TC:0 0 save_dt_nvmem_layout:875 nvmem[1] = cfg0_otp 0bit offset: 0, length: 8
D/TC:0 0 save_dt_nvmem_layout:875 nvmem[2] = part_number_otp 1bit offset: 0, length: 8
D/TC:0 0 save_dt_nvmem_layout:875 nvmem[3] = monotonic_otp 4bit offset: 0, length: 32
D/TC:0 0 save_dt_nvmem_layout:875 nvmem[4] = nand_otp 9bit offset: 0, length: 32
D/TC:0 0 save_dt_nvmem_layout:875 nvmem[5] = uid_otp 13bit offset: 0, length: 96
D/TC:0 0 save_dt_nvmem_layout:875 nvmem[6] = package_otp 16bit offset: 0, length: 32
D/TC:0 0 save_dt_nvmem_layout:875 nvmem[7] = hw2_otp 18bit offset: 0, length: 32
D/TC:0 0 save_dt_nvmem_layout:875 nvmem[8] = calib 23bit offset: 0, length: 16
D/TC:0 0 save_dt_nvmem_layout:875 nvmem[9] = calib 23bit offset: 16, length: 16
D/TC:0 0 save_dt_nvmem_layout:875 nvmem[10] = pkh_otp 24bit offset: 0, length: 256
D/TC:0 0 save_dt_nvmem_layout:875 nvmem[11] = mac 57bit offset: 0, length: 64
D/TC:0 0 save_dt_nvmem_layout:875 nvmem[12] = huk-otp 60bit offset: 0, length: 128
D/TC:0 0 call_initcalls:40 level 1 clk_dt_probe()
D/TC:0 0 clk_dt_probe:202 Probing clocks from devicetree
D/TC:0 0 clk_register:126 Registered clock clk-hse, freq 24000000
D/TC:0 0 probe_driver_node:443 element: fixed_clock on node clk-hse initialized
D/TC:0 0 clk_register:126 Registered clock clk-hsi, freq 64000000
D/TC:0 0 probe_driver_node:443 element: fixed_clock on node clk-hsi initialized
D/TC:0 0 clk_register:126 Registered clock clk-lse, freq 32768
D/TC:0 0 probe_driver_node:443 element: fixed_clock on node clk-lse initialized
D/TC:0 0 clk_register:126 Registered clock clk-lsi, freq 32000
D/TC:0 0 probe_driver_node:443 element: fixed_clock on node clk-lsi initialized
D/TC:0 0 clk_register:126 Registered clock clk-csi, freq 4000000
D/TC:0 0 probe_driver_node:443 element: fixed_clock on node clk-csi initialized
D/TC:0 0 clk_register:126 Registered clock (null), freq 266500000
D/TC:0 0 clk_register:126 Registered clock (null), freq 266500000
D/TC:0 0 clk_register:126 Registered clock (null), freq 266500000
D/TC:0 0 clk_register:126 Registered clock (null), freq 266500000
D/TC:0 0 clk_register:126 Registered clock (null), freq 533000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 533000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 133250000
D/TC:0 0 clk_register:126 Registered clock (null), freq 133250000
D/TC:0 0 clk_register:126 Registered clock (null), freq 266500000
D/TC:0 0 clk_register:126 Registered clock (null), freq 133250000
D/TC:0 0 clk_register:126 Registered clock (null), freq 133250000
D/TC:0 0 clk_register:126 Registered clock spi6, freq 66625000
D/TC:0 0 clk_register:126 Registered clock i2c4, freq 64000000
D/TC:0 0 clk_register:126 Registered clock i2c6, freq 64000000
D/TC:0 0 clk_register:126 Registered clock usart1, freq 66625000
D/TC:0 0 clk_register:126 Registered clock rtcapb, freq 66625000
D/TC:0 0 clk_register:126 Registered clock (null), freq 66625000
D/TC:0 0 clk_register:126 Registered clock (null), freq 66625000
D/TC:0 0 clk_register:126 Registered clock (null), freq 66625000
D/TC:0 0 clk_register:126 Registered clock iwdg, freq 66625000
D/TC:0 0 clk_register:126 Registered clock (null), freq 66625000
D/TC:0 0 clk_register:126 Registered clock (null), freq 24000000
D/TC:0 0 clk_register:126 Registered clock gpioz, freq 266500000
D/TC:0 0 clk_register:126 Registered clock crpy1, freq 266500000
D/TC:0 0 clk_register:126 Registered clock hash1, freq 266500000
D/TC:0 0 clk_register:126 Registered clock rng1, freq 4000000
D/TC:0 0 clk_register:126 Registered clock bkpsram, freq 266500000
D/TC:0 0 clk_register:126 Registered clock (null), freq 266500000
D/TC:0 0 clk_register:126 Registered clock rtc, freq 32768
D/TC:0 0 clk_register:126 Registered clock gpioa, freq 0
D/TC:0 0 clk_register:126 Registered clock gpiob, freq 0
D/TC:0 0 clk_register:126 Registered clock gpioc, freq 0
D/TC:0 0 clk_register:126 Registered clock gpiod, freq 0
D/TC:0 0 clk_register:126 Registered clock gpioe, freq 0
D/TC:0 0 clk_register:126 Registered clock gpiof, freq 0
D/TC:0 0 clk_register:126 Registered clock gpiog, freq 0
D/TC:0 0 clk_register:126 Registered clock gpioh, freq 0
D/TC:0 0 clk_register:126 Registered clock gpioi, freq 0
D/TC:0 0 clk_register:126 Registered clock gpioj, freq 0
D/TC:0 0 clk_register:126 Registered clock gpiok, freq 0
D/TC:0 0 clk_register:126 Registered clock (null), freq 208877928
D/TC:0 0 clk_register:126 Registered clock (null), freq 64000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 64000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 64000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 64000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 64000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 64000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 208877928
D/TC:0 0 clk_register:126 Registered clock (null), freq 64000000
D/TC:0 0 clk_register:126 Registered clock syscfg, freq 0
D/TC:0 0 clk_register:126 Registered clock (null), freq 0
D/TC:0 0 clk_register:126 Registered clock (null), freq 0
D/TC:0 0 clk_register:126 Registered clock dbg, freq 0
D/TC:0 0 clk_register:126 Registered clock hse, freq 24000000
D/TC:0 0 clk_register:126 Registered clock csi, freq 4000000
D/TC:0 0 clk_register:126 Registered clock lsi, freq 32000
D/TC:0 0 clk_register:126 Registered clock lse, freq 32768
D/TC:0 0 clk_register:126 Registered clock hsi, freq 64000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 12000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 650000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 650000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 650000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 266500000
D/TC:0 0 clk_register:126 Registered clock pll2q, freq 266500000
D/TC:0 0 clk_register:126 Registered clock pll2r, freq 533000000
D/TC:0 0 clk_register:126 Registered clock (null), freq 208877929
D/TC:0 0 clk_register:126 Registered clock pll3q, freq 24573874
D/TC:0 0 clk_register:126 Registered clock pll3r, freq 11290698
D/TC:0 0 clk_register:126 Registered clock (null), freq 266500000
D/TC:0 0 clk_register:126 Registered clock (null), freq 64000000
D/TC:0 0 clk_register:126 Registered clock mcu, freq 208877929
D/TC:0 0 probe_driver_node:443 element: stm32mp1_clock on node rcc@50000000 initialized
D/TC:0 0 call_initcalls:40 level 2 init_debug()
D/TC:0 0 stm32_bsec_find_otp_in_nvmem_layout:644 nvmem cfg0_otp = 0: 0 bit offset: 0, length: 8
I/TC: WARNING: All debug access are allowed
D/TC:0 0 call_initcalls:40 level 2 provisioning_probe()
D/TC:0 0 call_initcalls:40 level 2 probe_dt_drivers_early()
D/TC:0 0 add_node_to_probe:641 element: stm32-cpu-opp on node cpu0-opp-table
D/TC:0 0 add_node_to_probe:641 element: simple-bus on node soc
D/TC:0 0 add_node_to_probe:641 element: simple-bus on node ahb
D/TC:0 0 add_node_to_probe:641 element: fixed-regulator on node vin
D/TC:0 0 probe_driver_node:443 element: fixed-regulator on node vin initialized
D/TC:0 0 probe_driver_node:443 element: simple-bus on node ahb initialized
D/TC:0 0 add_node_to_probe:641 element: stm32mp15_rstctrl on node rcc@50000000
D/TC:0 0 add_node_to_probe:641 element: stm32mp1-pwr-regu on node pwr@50001000
D/TC:0 0 add_node_to_probe:641 element: stm32-rtc on node rtc@5c004000
D/TC:0 0 add_node_to_probe:641 element: stm32mp1-tzc400 on node tzc@5c006000
D/TC:0 0 add_node_to_probe:641 element: stm32-tamp on node tamp@5c00a000
D/TC:0 0 add_node_to_probe:641 element: stm32_gpio on node pin-controller@50002000
D/TC:0 0 add_node_to_probe:641 element: stm32_gpio on node pin-controller-z@54004000
D/TC:0 0 add_node_to_probe:641 element: stm32-etzpc on node etzpc@5c007000
D/TC:0 0 probe_driver_node:443 element: simple-bus on node soc initialized
D/TC:0 0 probe_driver_node:449 element: stm32-cpu-opp on node cpu0-opp-table deferred 1 time(s)
D/TC:0 0 probe_driver_node:449 element: stm32-cpu-opp on node cpu0-opp-table deferred 2 time(s)
D/TC:0 0 stm32_etzpc_set_driverdata:517 ETZPC revision 0x32, per_sec 96, ahb_sec 0, tzma 2
D/TC:0 0 add_node_to_probe:641 element: stm32_i2c on node i2c@5c002000
D/TC:0 0 probe_driver_node:443 element: stm32-etzpc on node etzpc@5c007000 initialized
D/TC:0 0 _fdt_stm32_gpio_controller:930 Bank name gpio@54004000
D/TC:0 0 _fdt_stm32_gpio_controller:982 GPIO bank Z assigned to non-secure
D/TC:0 0 stm32_gpio_parse_pinctrl_node:1146 Registered GPIO bank Z (8 pins) @d9004000
D/TC:0 0 probe_driver_node:443 element: stm32_gpio on node pin-controller-z@54004000 initialized
D/TC:0 0 _fdt_stm32_gpio_controller:930 Bank name gpio@50002000
D/TC:0 0 stm32_gpio_parse_pinctrl_node:1146 Registered GPIO bank A (16 pins) @d9402000
D/TC:0 0 _fdt_stm32_gpio_controller:930 Bank name gpio@50003000
D/TC:0 0 stm32_gpio_parse_pinctrl_node:1146 Registered GPIO bank B (16 pins) @d9403000
D/TC:0 0 _fdt_stm32_gpio_controller:930 Bank name gpio@50004000
D/TC:0 0 stm32_gpio_parse_pinctrl_node:1146 Registered GPIO bank C (16 pins) @d9404000
D/TC:0 0 _fdt_stm32_gpio_controller:930 Bank name gpio@50005000
D/TC:0 0 stm32_gpio_parse_pinctrl_node:1146 Registered GPIO bank D (16 pins) @d9405000
D/TC:0 0 _fdt_stm32_gpio_controller:930 Bank name gpio@50006000
D/TC:0 0 stm32_gpio_parse_pinctrl_node:1146 Registered GPIO bank E (16 pins) @d9406000
D/TC:0 0 _fdt_stm32_gpio_controller:930 Bank name gpio@50007000
D/TC:0 0 stm32_gpio_parse_pinctrl_node:1146 Registered GPIO bank F (16 pins) @d9407000
D/TC:0 0 _fdt_stm32_gpio_controller:930 Bank name gpio@50008000
D/TC:0 0 stm32_gpio_parse_pinctrl_node:1146 Registered GPIO bank G (16 pins) @d9408000
D/TC:0 0 _fdt_stm32_gpio_controller:930 Bank name gpio@50009000
D/TC:0 0 stm32_gpio_parse_pinctrl_node:1146 Registered GPIO bank H (16 pins) @d9409000
D/TC:0 0 _fdt_stm32_gpio_controller:930 Bank name gpio@5000a000
D/TC:0 0 stm32_gpio_parse_pinctrl_node:1146 Registered GPIO bank I (12 pins) @d940a000
D/TC:0 0 probe_driver_node:443 element: stm32_gpio on node pin-controller@50002000 initialized
D/TC:0 0 probe_driver_node:449 element: stm32-tamp on node tamp@5c00a000 deferred 1 time(s)
D/TC:0 0 tzc_set_driverdata:124 TZC400 Filters 2 Regions 8
D/TC:0 0 add_carved_out_nsec:382 0xc0000000 - 0xddffffff : Sec access 0 NS access 0x87fb87fb
D/TC:0 0 tzc_dump_state:473 region 0
D/TC:0 0 tzc_dump_state:476 region_base: 0x0000000000000000
D/TC:0 0 tzc_dump_state:479 region_top: 0x00000000ffffffff
D/TC:0 0 tzc_dump_state:481 secure rw: TZC_REGION_S_NONE
D/TC:0 0 tzc_dump_state:486 filter 0 enable
D/TC:0 0 tzc_dump_state:486 filter 1 enable
D/TC:0 0 tzc_dump_state:473 region 1
D/TC:0 0 tzc_dump_state:476 region_base: 0x00000000de000000
D/TC:0 0 tzc_dump_state:479 region_top: 0x00000000dfffffff
D/TC:0 0 tzc_dump_state:481 secure rw: TZC_REGION_S_RDWR
D/TC:0 0 tzc_dump_state:486 filter 0 enable
D/TC:0 0 tzc_dump_state:486 filter 1 enable
D/TC:0 0 tzc_dump_state:473 region 2
D/TC:0 0 tzc_dump_state:476 region_base: 0x00000000c0000000
D/TC:0 0 tzc_dump_state:479 region_top: 0x00000000ddffffff
D/TC:0 0 tzc_dump_state:481 secure rw: TZC_REGION_S_NONE
D/TC:0 0 tzc_dump_state:486 filter 0 enable
D/TC:0 0 tzc_dump_state:486 filter 1 enable
D/TC:0 0 gic_it_set_cpu_mask:350 cpu_mask: writing 0xff to 0xd8621824
D/TC:0 0 gic_it_set_cpu_mask:352 cpu_mask: 0x3
D/TC:0 0 gic_it_set_prio:361 prio: writing 0x1 to 0xd8621424
D/TC:0 0 probe_driver_node:443 element: stm32mp1-tzc400 on node tzc@5c006000 initialized
D/TC:0 0 probe_driver_node:443 element: stm32-rtc on node rtc@5c004000 initialized
D/TC:0 0 probe_driver_node:443 element: stm32mp1-pwr-regu on node pwr@50001000 initialized
D/TC:0 0 probe_driver_node:443 element: stm32mp15_rstctrl on node rcc@50000000 initialized
D/TC:0 0 probe_driver_node:449 element: stm32-tamp on node tamp@5c00a000 deferred 2 time(s)
D/TC:0 0 i2c_compute_timing:455 I2C SDADEL(min/max): 18/519, SCLDEL(Min): 285
D/TC:0 0 i2c_compute_timing:553 I2C TIMINGR (PRESC/SCLDEL/SDADEL): 1/8/1
D/TC:0 0 i2c_compute_timing:555 I2C TIMINGR (SCLH/SCLL): 27/38
D/TC:0 0 i2c_compute_timing:557 I2C TIMINGR: 0x10811b26
D/TC:0 0 i2c_setup_timing:644 I2C Freq(400000Hz), Clk Source(64000000)
D/TC:0 0 i2c_setup_timing:646 I2C Rise(185) and Fall(20) Time
D/TC:0 0 i2c_setup_timing:648 I2C Analog Filter(On), DNF(0)
D/TC:0 0 add_node_to_probe:641 element: stm32_pmic on node stpmic@33
D/TC:0 0 probe_driver_node:443 element: stm32_i2c on node i2c@5c002000 initialized
D/TC:0 0 probe_driver_node:449 element: stm32-cpu-opp on node cpu0-opp-table deferred 3 time(s)
D/TC:0 0 probe_driver_node:449 element: stm32-cpu-opp on node cpu0-opp-table deferred 4 time(s)
D/TC:0 0 register_periph:104 Register I2C4 as non-secure
D/TC:0 0 initialize_pmic:724 PMIC version = 0x21
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul buck1: enable, 1200mV
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul buck2: enable, 1350mV
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul buck3: enable, 3300mV
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul buck4: enable, 3300mV
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul ldo1: disable, 1800mV
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul ldo2: disable, 1800mV
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul ldo3: enable, 1700mV
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul ldo4: enable, 3300mV
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul ldo5: enable, 2900mV
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul ldo6: disable, 1000mV
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul vref_ddr: enable, 3300mV
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul boost: disable, 5000mV
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul pwr_sw1: disable, 5000mV
D/TC:0 0 stpmic1_dump_regulators:1137 PMIC regul pwr_sw2: disable, 5000mV
D/TC:0 0 parse_regulator_fdt_nodes:185 No CPU supply provided
D/TC:0 0 probe_driver_node:443 element: stm32_pmic on node stpmic@33 initialized
D/TC:0 0 probe_driver_node:449 element: stm32-tamp on node tamp@5c00a000 deferred 3 time(s)
D/TC:0 0 probe_driver_node:449 element: stm32-tamp on node tamp@5c00a000 deferred 4 time(s)
D/TC:0 0 probe_driver_node:449 element: stm32-cpu-opp on node cpu0-opp-table deferred 5 time(s)
D/TC:0 0 process_probe_list:590 Unresolved dependencies after 5 rounds, 5 deferred
D/TC:0 0 probe_dt_drivers_early:774 Deferred drivers probing
D/TC:0 0 print_probe_list:397 Probe list: 2 elements
D/TC:0 0 print_probe_list:399 |- Driver stm32-tamp probes on node tamp@5c00a000
D/TC:0 0 print_probe_list:399 |- Driver stm32-cpu-opp probes on node cpu0-opp-table
D/TC:0 0 print_probe_list:403 `- Probe list end
D/TC:0 0 print_probe_list:409 Failed list: 0 elements
D/TC:0 0 print_probe_list:414 `- Failed list end
D/TC:0 0 call_initcalls:40 level 3 platform_banner()
I/TC: Platform stm32mp1: flavor PLATFORM_FLAVOR - DT stm32mp151a-stm32-computer-firmware-mx.dts
I/TC: OP-TEE ST profile: system_services
D/TC:0 0 call_initcalls:40 level 3 init_stm32mp1_calib()
D/TC:0 0 stm32mp_start_clock_calib:406 HSI clock calibration not supported
D/TC:0 0 stm32mp_start_clock_calib:408 CSI clock calibration not supported
D/TC:0 0 call_initcalls:40 level 3 verify_pseudo_tas_conformance()
D/TC:0 0 call_initcalls:40 level 3 mobj_init()
D/TC:0 0 call_initcalls:40 level 3 default_mobj_init()
D/TC:0 0 call_initcalls:40 level 3 tee_cryp_init()
D/TC:0 0 call_initcalls:40 level 4 init_console_from_dt()
E/TC:0 0 assertion 'info.reg != DT_INFO_INVALID_REG && info.reg_size != DT_INFO_INVALID_REG_SIZE' failed at core/drivers/stm32_uart.c:156 <stm32_uart_init_from_dt_node>
E/TC:0 0 Panic at core/kernel/assert.c:28 <_assert_break>
E/TC:0 0 TEE load address @ 0xde000000
E/TC:0 0 Call stack:
E/TC:0 0 0xde002679
E/TC:0 0 0xde015517
E/TC:0 0 0xde01414f
E/TC:0 0 0xde00d4eb
E/TC:0 0 0xde00355d
E/TC:0 0 0xde01602d
E/TC:0 0 0xde00243d
E/TC:0 0 0xde00019c
D/TC:0 0 stm32_bsec_find_otp_in_nvmem_layout:644 nvmem part_number_otp = 1: 1 bit offset: 0, length: 8
M/TC: CPU : 0
M/TC: usr_sp : 0x04480382
M/TC: usr_lr : 0x1000c804
M/TC: irq_spsr : 0x00021488
M/TC: irq_sp : 0x48200010
M/TC: irq_lr : 0x020a1498
M/TC: fiq_spsr : 0x18000830
M/TC: fiq_sp : 0x0bc61000
M/TC: fiq_lr : 0x40000000
M/TC: svc_spsr : 0x010a0483
M/TC: svc_sp : 0x30001010
M/TC: svc_lr : 0x00200501
M/TC: abt_spsr : 0x00484800
M/TC: abt_sp : 0x04080282
M/TC: abt_lr : 0xc800c010
M/TC: und_spsr : 0x24020403
M/TC: und_sp : 0x10145010
M/TC: und_lr : 0x09090400
M/TC: pmcr : 0x08008004
2024-08-08 3:12 PM - edited 2024-08-08 4:20 PM
I tried to add &uart4 inside the .dts file (here) of Op-tee folder inside the Device Tree folder.
I don't know if uart4 should be there. It's not generated by CubeIDE.
/* USER CODE BEGIN addons */
&uart4 {
pinctrl-names = "default", "sleep", "idle";
pinctrl-0 = <&uart4_pins_a>;
pinctrl-1 = <&uart4_sleep_pins_a>;
pinctrl-2 = <&uart4_idle_pins_a>;
/delete-property/dmas;
/delete-property/dma-names;
status = "okay";
};
/* USER CODE END addons */
Here is the code snippet where it fails.
#ifdef CFG_EMBED_DTB
static TEE_Result init_console_from_dt(void)
{
struct stm32_uart_pdata *pd = NULL;
void *fdt = NULL;
int node = 0;
TEE_Result res = TEE_ERROR_GENERIC;
fdt = get_embedded_dt();
res = get_console_node_from_dt(fdt, &node, NULL, NULL);
if (res == TEE_ERROR_ITEM_NOT_FOUND) {
fdt = get_external_dt();
res = get_console_node_from_dt(fdt, &node, NULL, NULL);
if (res == TEE_ERROR_ITEM_NOT_FOUND)
return TEE_SUCCESS;
if (res != TEE_SUCCESS)
return res;
}
pd = stm32_uart_init_from_dt_node(fdt, node); <----- Error
struct stm32_uart_pdata *stm32_uart_init_from_dt_node(void *fdt, int node)
{
TEE_Result res = TEE_ERROR_GENERIC;
struct stm32_uart_pdata *pd = NULL;
struct dt_node_info info = { };
uint32_t cfg8 = 0;
_fdt_fill_device_info(fdt, &info, node);
if (info.status == DT_STATUS_DISABLED)
return NULL;
assert(info.reg != DT_INFO_INVALID_REG &&
info.reg_size != DT_INFO_INVALID_REG_SIZE); <--- Error
If we are looking at the stm32mp151.dtsi here ,of Op-tee, we can see it contains reg.
uart4: serial@40010000 {
compatible = "st,stm32h7-uart";
reg = <0x40010000 0x400>;
interrupts-extended = <&exti 30 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&rcc UART4_K>;
wakeup-source;
dmas = <&dmamux1 63 0x400 0x15>,
<&dmamux1 64 0x400 0x11>;
dma-names = "rx", "tx";
resets = <&rcc UART4_R>;
status = "disabled";
};
In this case, reg must be 0x4001000 and reg_size must be 0x400 I guess.
So why does this error occurs?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.