2024-04-27 5:31 AM
Hello
Iam Using Stm32mp157aaa3 processor in my custom board and U boot version 2023.10.Can we load .bin extension file using rproc command in uboot.
Tanks & Regards
Srikanth.R
2024-05-03 6:29 AM
Hello Srikanth,
Yes only ELF format is supported because it contains information about binary location you don't have obviously in the .bin format.
By the way, we support .bin firmware but in this case this is for firmware signed (so for authentication at start up) because this binary is associated with additional tables. But My understanding is not what you want to do (if you are interested, the wiki is describing this more complex use case...).
Also note, on V5 release there was a regression on the feature (M4 load from U-boot). It was solved with this patch:
https://github.com/STMicroelectronics/linux/commit/89fdf7bece3d1be0d37156897ed8e183d5fcf1e4
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.