cancel
Showing results for 
Search instead for 
Did you mean: 

Latest supported version of Chromium

hiba
Associate

Hello,


I want to know what is the latest Chromium version supported by OpenST Linux on Scarthgap.
Do we have GPU acceleration on it?

Thank you in advance,

Hiba

 

@PPAGE.13

@Billy OWEN 

@Gregory PLANCHON 

5 REPLIES 5
DMårt
Lead

@hiba 

The ST Dev Team is working on a solution for that. 

They said they will find a solution in half of 2025.

What ST have tried is to build a minimal chromium web browser by using Qt Web Engine, which use the same web engine as Chromium. They have run that Qt Nano Web browser in kiosk mode, e.g no buttons and input text boxes. It works like a charm.

My advice is to look for Gentoo Use flags to see what you can use with compilation for Firefox. They have a lot of flags you can use to optimize a web browser by using the same web engine as Firefox is using.

I'm working on a Github project for creating an optimal web browser for MP2.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer

 

I am currently working on bringing up Chromium on a custom board based on STM32MP255C, using OpenSTLinux 6.2 (Scarthgap).

Context

  1. Platform: STM32MP255C (custom board)

  2. Distribution: OpenSTLinux 6.2 (Scarthgap)

  3. Goal: Run a Chromium-based browser with GPU acceleration (Wayland/Weston or equivalent)


Questions

  1. Chromium support status

    • What is the latest Chromium version officially supported on OpenSTLinux 6.2 for STM32MP25?

    • Is there any validated configuration for Chromium on this platform?

  2. Layer availability

    • Does ST provide or maintain a Yocto layer (meta-chromium or equivalent) compatible with OpenSTLinux 6.2?

    • If yes, could you share:

      • the repository

      • the branch

      • or the exact commit used internally

  3. GPU acceleration

    • Is GPU acceleration supported with Chromium on STM32MP25?

    • If yes:

      • which backend is expected (Wayland, X11, EGL, Ozone-Wayland, etc.)?

      • are there specific patches or configurations required?

  4. Recommended approach

    • Is Chromium currently a supported use case, or is the recommended approach still:

      • Qt WebEngine

      • or another browser stack?


Additional information

I noticed discussions indicating that Chromium support is still under development for MP25. I would like to understand the current official position and whether there is any internal or experimental layer already available for OpenSTLinux 6.2.


Thank you in advance for your support.

BR,
Yassine 

@DMårt 

From my side, I have the impression that we still do not have a clear answer.

If ST already has an internal Chromium layer, branch, patches, or a validated configuration, even experimental, it would be very useful to share it with the community.

At least then we could test it, contribute, report issues, and help move the subject forward.

For now, it feels like the topic exists internally, but there is no public repository or concrete reference that users can build from, which is quite disappointing.

So yes, I am also very interested in the current status, especially whether Chromium is realistically usable on MP2 with GPU acceleration or not.

Best regards,

Yassine

@Yassine_behilil @hiba 

WPEWebKit have a meta layer for a web browser suitable for embedded systems.

I have spoke to WPEWebKit and they are really interested to build and configure a solution for the STM32MP2 processor.

I think ST have other things they need to be focusing on e.g bug fixes are prio #1.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer

@victoria61943 

Have you tried to build a web browser for STM32MP257?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer