2020-04-28 5:00 PM
I am using starter image "en.st-android-10.0.0-2020-02-21-eval-sd-starter.tar.gz".
CubeProgrammer gave me "Error: an error occurred while uploading data from the virtual partition 0xF1" . Below is full log:
16:56:19 : USB speed : High Speed (480MBit/s)
16:56:19 : Manuf. ID : STMicroelectronics
16:56:19 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
16:56:19 : SN : 0046003E3338510634383330
16:56:19 : FW version : 0x0110
16:56:19 : Device ID : 0x0500
16:56:23 : Start Embedded Flashing service
16:56:23 : Memory Programming ...
16:56:23 : Opening and parsing file: fsbl-programmer.img
16:56:23 : File : fsbl-programmer.img
16:56:23 : Size : 245360 Bytes
16:56:23 : Partition ID : 0x01
16:56:23 : Download in Progress:
16:56:24 : File download complete
16:56:24 : Time elapsed during download operation: 00:00:00.431
16:56:24 : RUNNING Program ...
16:56:24 : PartID: :0x01
16:58:14 : Error: an error occured while uploading data from the virtual partition 0xF1
16:58:14 : Start operation done successfully at partition 0x01
Solved! Go to Solution.
2020-11-11 2:55 AM
Hello Mr. @Nicolas L
thank you so much for your instructions,
may you help me solve this issue please, when you have time.
[ 6% 4099/66511] build fsbl.img
FAILED: fsbl.img
/bin/bash -c "(prebuilts/build-tools/linux-x86/bin/acp -fp device/stm/stm32mp1-bootloader/prebuilt/fsbl/tf-a-stm32mp157c-dk2-trusted.stm32 out/target/product/disco/fsbl-trusted.img ) && (prebuilts/build-tools/linux-x86/bin/acp -fp device/stm/stm32mp1-bootloader/prebuilt/fsbl/tf-a-stm32mp157c-dk2-optee.stm32 out/target/product/disco/fsbl-optee.img ) && (prebuilts/build-tools/linux-x86/bin/acp -fp device/stm/stm32mp1-bootloader/prebuilt/fsbl/tf-a-stm32mp157c-dk2-programmer.stm32 out/target/product/disco/fsbl-programmer.img )"
acp: file 'device/stm/stm32mp1-bootloader/prebuilt/fsbl/tf-a-stm32mp157c-dk2-programmer.stm32' does not exist
[ 6% 4101/66511] Build hyb out/target/product/disco/obj/ETC/hyph-nn_intermediates/hyph-nn.hyb <- external/hyphenation-patterns/nn//hyph-nn.pat.txt
12585 unique nodes, 42861 total
[ 6% 4102/66511] Build hyb out/target/product/disco/obj/ETC/hyph-nb_intermediates/hyph-nb.hyb <- external/hyphenation-patterns/nb//hyph-nb.pat.txt
12585 unique nodes, 42861 total
[ 6% 4104/66511] Build hyb out/target/product/disco/obj/ETC/hyph-hu_intermediates/hyph-hu.hyb <- external/hyphenation-patterns/hu//hyph-hu.pat.txt
21515 unique nodes, 102669 total
11:27:48 ninja failed with: exit status 1
#### failed to build some targets (02:41 (mm:ss)) ####
2022-03-18 1:27 AM
Hi @Nicolas L (ST Employee)
It's possible to receive those sources and directives too?
Thanks a lot,
Patrick
2022-03-18 1:45 AM
The other option to fix Chrome can't download images on Android is to clear its data and cache. Doing so will reset the browser to default settings. However, it will not delete your downloaded data. Open Settings on your phone.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.