2026-03-06 1:45 PM
Section 5.1.1 Step 3 says that
Copy the dts file from the directory: x-linux-gnss1-app\linux-kernel\patch\5.15\kernel to the kernel
source directory at <KERNEL SOURCE PATH>/ arch/arm/boot/dts/
But in the latest X-LINUX-GNSS1 package, the linux kernel is 6.1.11 and there are 3 patch files and 1 fragment file is present.
It is unclear what to copy exactly.
2026-04-06 1:38 AM
Hello @embeddedbro ,
The Device tree and kernel patches are provided in the 6.1 directory. You can apply them.
Regards,
S
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.