2026-02-07 9:05 AM
I got a panic message from drivers/st/clk/clk-stm32-core.c at Trusted Firmware.
My question is: What is clock ID 5? Is that MSI clock or LSE clock?
Is there any information I could read about this ID?
int clk_stm32_enable_call_ops(struct stm32_clk_priv *priv, uint16_t id)
{
const struct stm32_clk_ops *ops = _clk_get_ops(priv, id);
if ((ops->is_enabled != NULL) && ops->is_enabled(priv, id)) {
return 0;
}
if (ops->enable != NULL) {
ops->enable(priv, id);
}
if ((ops->is_enabled != NULL) && !ops->is_enabled(priv, id)) {
ERROR("failed to enable clock id: %u\n", id);
panic();
}
return 0;
}
The output is
NOTICE: Early console setup
ERROR: failed to enable clock id: 5
BACKTRACE: START: clk_stm32_enable_call_ops
0: EL3: 0xe017bac
1: EL3: 0xe01be2c
2: EL3: 0xe01beb0
3: EL3: 0xe01bf54
4: EL3: 0xe01c240
5: EL3: 0xe01db28
6: EL3: 0xe029a2c
7: EL3: 0xe0170dc
BACKTRACE: END: clk_stm32_enable_call_ops
PANIC at PC : 0x000000000e01be34
2026-02-08 11:32 PM
2026-02-09 12:30 AM
It's for STM32MP257, not STM32MP157.
2026-02-09 12:58 AM
Sorry for mixed-up.
So, definitely not I2S_CLK as per https://github.com/STMicroelectronics/arm-trusted-firmware/blob/v2.10-stm32mp/include/dt-bindings/clock/stm32mp25-clks.h
Probably not MSI (which is internal).
It could be LSE (e.g. fail to start oscillator), but not sure it is used in TF-A.
Are you sure about HSE oscillation and setup in DT ?
Regards
2026-02-09 1:12 AM
It seems that LSE and HSE is disabled already in TF-A. I'm guessing that it could be some settings in DT tyst should be default in CubeMX, but it isin't.
* https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
*/
/dts-v1/;
#include <dt-bindings/pinctrl/stm32-pinfunc.h>
#include <dt-bindings/clock/stm32mp25-clksrc.h>
#include "stm32mp25-mx.dtsi"
#include "stm32mp257.dtsi"
#include "stm32mp25xf.dtsi"
#include "stm32mp257f-firmware-mx-rcc.dtsi"
#include "stm32mp25xxak-pinctrl.dtsi"
#include "stm32mp25-ddr.dtsi"
/* USER CODE BEGIN includes */
/* USER CODE END includes */
/ {
model = "STMicroelectronics custom STM32CubeMX board - openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11";
compatible = "st,stm32mp257f-firmware-mx", "st,stm32mp257";
memory@80000000 {
device_type = "memory";
reg = <0x0 0x80000000 0x00000001 0x00000000>;
/* USER CODE BEGIN memory */
/* USER CODE END memory */
};
/* USER CODE BEGIN root */
aliases{
serial0 = &usart2;
};
chosen{
stdout-path = "serial0:115200n8";
};
/* USER CODE END root */
}; /*root*/
&pinctrl {
i2c7_pins_mx: i2c7_mx-0 {
pins {
pinmux = <STM32_PINMUX('D', 14, AF10)>, /* I2C7_SDA */
<STM32_PINMUX('D', 15, AF10)>; /* I2C7_SCL */
bias-disable;
drive-open-drain;
slew-rate = <0>;
};
};
sdmmc1_pins_mx: sdmmc1_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('E', 0, AF10)>, /* SDMMC1_D2 */
<STM32_PINMUX('E', 1, AF10)>, /* SDMMC1_D3 */
<STM32_PINMUX('E', 2, AF10)>, /* SDMMC1_CMD */
<STM32_PINMUX('E', 4, AF10)>, /* SDMMC1_D0 */
<STM32_PINMUX('E', 5, AF10)>; /* SDMMC1_D1 */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('E', 3, AF10)>; /* SDMMC1_CK */
bias-disable;
drive-push-pull;
slew-rate = <3>;
};
};
usart2_pins_mx: usart2_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 15, AF6)>; /* USART2_RX */
bias-disable;
drive-push-pull;
};
pins2 {
pinmux = <STM32_PINMUX('C', 1, AF6)>; /* USART2_TX */
bias-disable;
drive-push-pull;
slew-rate = <0>;
};
};
/* USER CODE BEGIN pinctrl */
/* USER CODE END pinctrl */
};
&pinctrl_z {
/* USER CODE BEGIN pinctrl_z */
/* USER CODE END pinctrl_z */
};
&bsec {
status = "okay";
/* USER CODE BEGIN bsec */
board_id: board_id@3d8 {
reg = <0x3d8 0x4>;
};
/* USER CODE END bsec */
};
&ddr {
status = "okay";
/* USER CODE BEGIN ddr */
vdd1-supply = <&vdd1_ddr>;
vdd2-supply = <&vdd2_ddr>;
vddq-supply = <&vdd2_ddr>;
/* USER CODE END ddr */
};
&i2c7 {
pinctrl-names = "default";
pinctrl-0 = <&i2c7_pins_mx>;
status = "okay";
/* USER CODE BEGIN i2c7 */
i2c-scl-rising-time-ns = <185>;
i2c-scl-falling-time-ns = <20>;
clock-frequency = <400000>;
#address-cells = <1>;
#size-cells = <0>;
pmic2: stpmic@33 {
compatible = "st,stpmic2";
reg = <0x33>;
status = "okay";
regulators {
compatible = "st,stpmic2-regulators";
vddcpu: buck1 {
regulator-name = "vddcpu";
regulator-min-microvolt = <800000>;
regulator-max-microvolt = <910000>;
regulator-always-on;
};
vddcore: buck2 {
regulator-name = "vddcore";
regulator-min-microvolt = <820000>;
regulator-max-microvolt = <820000>;
regulator-always-on;
};
vddgpu: buck3 {
regulator-name = "vddgpu";
regulator-min-microvolt = <800000>;
regulator-max-microvolt = <900000>;
regulator-always-on;
};
vddio_pmic: buck4 {
regulator-name = "vddio_pmic";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
v1v8: buck5 {
regulator-name = "v1v8";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-always-on;
};
vdd2_ddr: buck6 {
regulator-name = "vdd2_ddr";
regulator-min-microvolt = <1100000>;
regulator-max-microvolt = <1100000>;
};
v3v3: buck7 {
regulator-name = "v3v3";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
vdda1v8_aon: ldo1 {
regulator-name = "vdda1v8_aon";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-always-on;
};
vdd_emmc: ldo2 {
regulator-name = "vdd_SD_card_temporary";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
vdd1_ddr: ldo3 {
regulator-name = "vdd1_ddr";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
};
vdd3v3_usb: ldo4 {
regulator-name = "vdd3v3_usb";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
v5v_hdmi: ldo5 {
regulator-name = "v5v_hdmi";
regulator-min-microvolt = <2000000>;
regulator-max-microvolt = <2000000>;
};
vdd_sdcard: ldo7 {
regulator-name = "vdd_sdcard";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
vddio_sdcard: ldo8 {
regulator-name = "vddio_sdcard";
st,regulator-bypass-microvolt = <3300000>;
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
};
};
/* USER CODE END i2c7 */
};
&icache {
status = "okay";
/* USER CODE BEGIN icache */
/* USER CODE END icache */
};
&rcc {
status = "okay";
/* USER CODE BEGIN rcc */
/* USER CODE END rcc */
};
&sdmmc1 {
pinctrl-names = "default";
pinctrl-0 = <&sdmmc1_pins_mx>;
status = "okay";
/* USER CODE BEGIN sdmmc1 */
st,neg-edge;
bus-width = <4>;
vmmc-supply = <&vdd_sdcard>;
vqmmc-supply = <&vddio1>;
/delete-property/cap-sd-highspeed;
/delete-property/cap-mmc-highspeed;
/* USER CODE END sdmmc1 */
};
&usart2 {
pinctrl-names = "default";
pinctrl-0 = <&usart2_pins_mx>;
status = "okay";
/* USER CODE BEGIN usart2 */
/* USER CODE END usart2 */
};
/* USER CODE BEGIN addons */
/* USER CODE END addons */ * https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
*/
&clk_lsi {
clock-frequency = <32000>;
/* USER CODE BEGIN clk_lsi */
/* USER CODE END clk_lsi */
};
&clk_hsi {
clock-frequency = <64000000>;
/* USER CODE BEGIN clk_hsi */
/* USER CODE END clk_hsi */
};
&clk_msi {
clock-frequency = <16000000>;
/* USER CODE BEGIN clk_msi */
/* USER CODE END clk_msi */
};
&clk_lse {
status = "disabled";
/* USER CODE BEGIN clk_lse */
/* USER CODE END clk_lse */
};
&clk_hse {
status = "disabled";
/* USER CODE BEGIN clk_hse */
/* USER CODE END clk_hse */
};
&rcc {
st,flexgen = <
FLEXGEN_CFG(0, XBAR_SRC_HSI, 0, 0)
FLEXGEN_CFG(1, XBAR_SRC_HSI, 0, 0)
FLEXGEN_CFG(2, XBAR_SRC_HSI, 0, 0)
FLEXGEN_CFG(3, XBAR_SRC_HSI, 0, 0)
FLEXGEN_CFG(4, XBAR_SRC_HSI, 0, 0)
FLEXGEN_CFG(5, XBAR_SRC_HSI, 0, 0)
FLEXGEN_CFG(6, XBAR_SRC_HSI, 0, 0)
FLEXGEN_CFG(8, XBAR_SRC_HSI_KER, 0, 0)
FLEXGEN_CFG(15, XBAR_SRC_HSI_KER, 0, 0)
FLEXGEN_CFG(33, XBAR_SRC_HSI_KER, 0, 0)
FLEXGEN_CFG(43, XBAR_SRC_HSI_KER, 0, 24)
FLEXGEN_CFG(44, XBAR_SRC_HSI_KER, 0, 7)
FLEXGEN_CFG(45, XBAR_SRC_HSI_KER, 0, 3)
FLEXGEN_CFG(51, XBAR_SRC_HSI_KER, 0, 0)
FLEXGEN_CFG(63, XBAR_SRC_HSI_KER, 0, 0)
>;
st,busclk = <
DIV_CFG(DIV_LSMCU, 0)
DIV_CFG(DIV_APB1, 0)
DIV_CFG(DIV_APB2, 0)
DIV_CFG(DIV_APB3, 0)
DIV_CFG(DIV_APB4, 0)
DIV_CFG(DIV_APBDBG, 0)
>;
st,kerclk = <
MUX_CFG(MUX_D3PER, MUX_D3PER_MSI)
>;
pll1:st,pll-1 {
st,pll = <&pll1_cfg_2176MHz>;
pll1_cfg_2176MHz: pll1-cfg-2176MHz{
cfg = <34 1 1 1>;
src=<MUX_CFG(MUX_MUXSEL5, MUXSEL_HSI)>;
};
/* USER CODE BEGIN pll1 */
/* USER CODE END pll1 */
};
pll2:st,pll-2 {
st,pll = <&pll2_cfg_600MHz>;
pll2_cfg_600MHz: pll2-cfg-600MHz{
cfg = <37 1 1 4>;
src=<MUX_CFG(MUX_MUXSEL6, MUXSEL_HSI)>;
frac = < 0x800000 >;
};
/* USER CODE BEGIN pll2 */
/* USER CODE END pll2 */
};
pll8:st,pll-8 {
st,pll = <&pll8_cfg_2176MHz>;
pll8_cfg_2176MHz: pll8-cfg-2176MHz{
cfg = <34 1 1 1>;
src=<MUX_CFG(MUX_MUXSEL4, MUXSEL_HSI)>;
};
/* USER CODE BEGIN pll8 */
/* USER CODE END pll8 */
};
/* USER CODE BEGIN rcc */
/* USER CODE END rcc */
}; #include "stm32mp25-fw-config.dtsi"
/ {
st-mem-firewall {
bl31_context: bl31-context@81fc0000 {
reg = <0x0 0x81fc0000 0x0 0x40000>;
st,protreg = <RISAFPROT(RISAF_REG_ID(7), 0, RIF_UNUSED, RIF_UNUSED, RIF_NSEC, RIF_ENC_DIS, RIF_BREN_EN)>;
};
op_tee: op-tee@82000000 {
reg = <0x0 0x82000000 0x0 0x2000000>;
st,protreg = <RISAFPROT(RISAF_REG_ID(8), 0, RIF_UNUSED, RIF_UNUSED, RIF_NSEC, RIF_ENC_DIS, RIF_BREN_EN)>;
};
};
/* USER CODE BEGIN root */
/* USER CODE END root */
}; * Copyright (C) 2026, STMicroelectronics - All Rights Reserved
* Author: STM32CubeMX code generation for STMicroelectronics.
*/
/* For more information on Device Tree configuration, please refer to
* https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
*/
#include "stm32mp25-fw-config.dtsi"
/ {
st-mem-firewall {
bl31_context: bl31-context@81fc0000 {
reg = <0x0 0x81fc0000 0x0 0x40000>;
st,protreg = <RISAFPROT(RISAF_REG_ID(7), 0, RIF_UNUSED, RIF_UNUSED, RIF_NSEC, RIF_ENC_DIS, RIF_BREN_EN)>;
};
op_tee: op-tee@82000000 {
reg = <0x0 0x82000000 0x0 0x2000000>;
st,protreg = <RISAFPROT(RISAF_REG_ID(8), 0, RIF_UNUSED, RIF_UNUSED, RIF_NSEC, RIF_ENC_DIS, RIF_BREN_EN)>;
};
};
/* USER CODE BEGIN root */
/* USER CODE END root */
};
2026-02-09 1:14 AM - edited 2026-02-09 1:16 AM
Here is a longer output of the error message. I think there is something in the DT that are missing.
NOTICE: Early console setup
mmap:
VA:0xe017000 PA:0xe017000 size:0x21000 attr:0x2 granularity:0x40000000
VA:0xe000000 PA:0xe000000 size:0x40000 attr:0x4a granularity:0x40000000
VA:0xe040000 PA:0xe040000 size:0x10000 attr:0x4a granularity:0x40000000
VA:0x40000000 PA:0x40000000 size:0x40000000 attr:0x48 granularity:0x40000000
VERBOSE: Translation tables state:
VERBOSE: Xlat regime: EL3
VERBOSE: Max allowed PA: 0x1ffffffff
VERBOSE: Max allowed VA: 0x1ffffffff
VERBOSE: Max mapped PA: 0x7fffffff
VERBOSE: Max mapped VA: 0x7fffffff
VERBOSE: Initial lookup level: 1
VERBOSE: Entries @initial lookup level: 8
VERBOSE: Used 2 sub-tables out of 4 (spare: 2)
[LV1] VA:0x0 size:0x40000000
[LV2] VA:0x0 size:0x200000
[LV2] (111 invalid descriptors omitted)
[LV2] VA:0xe000000 size:0x200000
[LV3] VA:0xe000000 PA:0xe000000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe001000 PA:0xe001000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe002000 PA:0xe002000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe003000 PA:0xe003000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe004000 PA:0xe004000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe005000 PA:0xe005000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe006000 PA:0xe006000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe007000 PA:0xe007000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe008000 PA:0xe008000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe009000 PA:0xe009000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe00a000 PA:0xe00a000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe00b000 PA:0xe00b000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe00c000 PA:0xe00c000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe00d000 PA:0xe00d000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe00e000 PA:0xe00e000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe00f000 PA:0xe00f000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe010000 PA:0xe010000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe011000 PA:0xe011000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe012000 PA:0xe012000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe013000 PA:0xe013000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe014000 PA:0xe014000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe015000 PA:0xe015000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe016000 PA:0xe016000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe017000 PA:0xe017000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe018000 PA:0xe018000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe019000 PA:0xe019000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe01a000 PA:0xe01a000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe01b000 PA:0xe01b000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe01c000 PA:0xe01c000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe01d000 PA:0xe01d000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe01e000 PA:0xe01e000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe01f000 PA:0xe01f000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe020000 PA:0xe020000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe021000 PA:0xe021000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe022000 PA:0xe022000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe023000 PA:0xe023000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe024000 PA:0xe024000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe025000 PA:0xe025000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe026000 PA:0xe026000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe027000 PA:0xe027000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe028000 PA:0xe028000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe029000 PA:0xe029000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe02a000 PA:0xe02a000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe02b000 PA:0xe02b000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe02c000 PA:0xe02c000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe02d000 PA:0xe02d000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe02e000 PA:0xe02e000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe02f000 PA:0xe02f000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe030000 PA:0xe030000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe031000 PA:0xe031000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe032000 PA:0xe032000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe033000 PA:0xe033000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe034000 PA:0xe034000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe035000 PA:0xe035000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe036000 PA:0xe036000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe037000 PA:0xe037000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0xe038000 PA:0xe038000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe039000 PA:0xe039000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe03a000 PA:0xe03a000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe03b000 PA:0xe03b000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe03c000 PA:0xe03c000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe03d000 PA:0xe03d000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe03e000 PA:0xe03e000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe03f000 PA:0xe03f000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe040000 PA:0xe040000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe041000 PA:0xe041000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe042000 PA:0xe042000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe043000 PA:0xe043000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe044000 PA:0xe044000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe045000 PA:0xe045000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe046000 PA:0xe046000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe047000 PA:0xe047000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe048000 PA:0xe048000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe049000 PA:0xe049000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe04a000 PA:0xe04a000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe04b000 PA:0xe04b000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe04c000 PA:0xe04c000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe04d000 PA:0xe04d000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe04e000 PA:0xe04e000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe04f000 PA:0xe04f000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0xe050000 size:0x1000
[LV3] (431 invalid descriptors omitted)
[LV2] VA:0xe200000 size:0x200000
[LV2] (398 invalid descriptors omitted)
[LV1] VA:0x40000000 PA:0x40000000 size:0x40000000 DEV-RW-XN-S
[LV1] VA:0x80000000 size:0x40000000
[LV1] (5 invalid descriptors omitted)
VERBOSE: Couldn't find property st,drive in dtb
VERBOSE: Couldn't find property st,drive in dtb
VERBOSE: Couldn't find property st,drive in dtb
VERBOSE: Couldn't find property st,drive in dtb
VERBOSE: Couldn't find property csg in dtb
VERBOSE: Couldn't find property frac in dtb
VERBOSE: Couldn't find property csg in dtb
VERBOSE: Couldn't find property frac in dtb
VERBOSE: Couldn't find property csg in dtb
VERBOSE: Couldn't find property frac in dtb
VERBOSE: Generic delay timer configured with mult=1 and div=64
ERROR: failed to enable clock id: 5
BACKTRACE: START: clk_stm32_enable_call_ops
0: EL3: 0xe017bac
1: EL3: 0xe01c210
2: EL3: 0xe01c294
3: EL3: 0xe01c338
4: EL3: 0xe01c640
5: EL3: 0xe01df28
6: EL3: 0xe02b118
7: EL3: 0xe0170dc
BACKTRACE: END: clk_stm32_enable_call_ops
PANIC at PC : 0x000000000e01c218
2026-02-09 5:37 AM - edited 2026-02-09 5:37 AM
Hi,
maybe there is some missing DT information expected as mandatory by TF-A
Altough not seen in https://github.com/STMicroelectronics/arm-trusted-firmware/blob/v2.10-stm32mp/fdts/stm32mp257f-ev1-ca35tdcid-rcc.dtsi
It might be elsewhere (missing 'include' somewhere ?)
Sorry not helping more. This is out of my knowledge.
Regards.
2026-02-11 3:24 PM
Yes. LSE was ID 5. But I don't know if I'm in need of LSE. I don't have any RTC or tamper activated. I have not even LSE activated at all.
NOTICE: Early console setup
NOTICE: clk_stm32_get_oscillator_name: id = 0
NOTICE: clk_stm32_get_oscillator_name: id = 1
NOTICE: clk_stm32_get_oscillator_name: id = 2
NOTICE: clk_stm32_get_oscillator_name: id = 3
NOTICE: clk_stm32_get_oscillator_name: id = 4
NOTICE: clk_stm32_get_oscillator_name: id = 5
NOTICE: clk_stm32_get_oscillator_name: id = 6
NOTICE: clk_stm32_init: priv->num = 152
NOTICE: clk_stm32_init: i = 0
NOTICE: clk_stm32_init: i = 1
NOTICE: clk_stm32_init: ops->init(priv, 1)
NOTICE: clk_stm32_osc_init: id = 1, name = clk-hsi
NOTICE: clk_stm32_init: i = 2
NOTICE: clk_stm32_init: ops->init(priv, 2)
NOTICE: clk_stm32_osc_init: id = 2, name = clk-hse
NOTICE: clk_stm32_init: i = 3
NOTICE: clk_stm32_init: ops->init(priv, 3)
NOTICE: clk_stm32_osc_init: id = 3, name = clk-msi
NOTICE: clk_stm32_init: i = 4
NOTICE: clk_stm32_init: ops->init(priv, 4)
NOTICE: clk_stm32_osc_init: id = 4, name = clk-lsi
NOTICE: clk_stm32_init: i = 5
NOTICE: clk_stm32_init: ops->init(priv, 5)
NOTICE: clk_stm32_osc_init: id = 5, name = clk-lse
NOTICE: clk_stm32_init: i = 6
NOTICE: clk_stm32_init: ops->init(priv, 6)
NOTICE: clk_stm32_osc_init: id = 6, name = i2s_ckin
NOTICE: clk_stm32_init: i = 7
NOTICE: clk_stm32_init: ops->init(priv, 7)
NOTICE: clk_stm32_osc_init: id = 7, name = spdif_symb
NOTICE: clk_stm32_init: i = 8
NOTICE: clk_stm32_init: i = 9
NOTICE: clk_stm32_init: i = 10
...
NOTICE: clk_stm32_init: i = 151
NOTICE: _clk_stm32_enable: CLK Lock
NOTICE: _clk_stm32_enable_core: if (parent != CLK_IS_ROOT)
NOTICE: _clk_stm32_enable_core: Calling clk_stm32_enable_call_ops
NOTICE: clk_stm32_enable_call_ops: Enabling with id = 2
NOTICE: _clk_stm32_enable_core: Increase priv->gate_refcounts[2] from 0 to 1
NOTICE: _clk_stm32_enable: CLK Unlock: 0
NOTICE: _clk_stm32_enable: CLK Lock
NOTICE: _clk_stm32_enable_core: if (parent != CLK_IS_ROOT)
NOTICE: _clk_stm32_enable_core: Calling clk_stm32_enable_call_ops
NOTICE: clk_stm32_enable_call_ops: Enabling with id = 3
NOTICE: _clk_stm32_enable_core: Increase priv->gate_refcounts[3] from 0 to 1
NOTICE: _clk_stm32_enable: CLK Unlock: 0
NOTICE: _clk_stm32_enable: CLK Lock
NOTICE: _clk_stm32_enable_core: if (parent != CLK_IS_ROOT)
NOTICE: _clk_stm32_enable_core: Calling clk_stm32_enable_call_ops
NOTICE: clk_stm32_enable_call_ops: Enabling with id = 4
NOTICE: _clk_stm32_enable_core: Increase priv->gate_refcounts[4] from 0 to 1
NOTICE: _clk_stm32_enable: CLK Unlock: 0
NOTICE: _clk_stm32_enable: CLK Lock
NOTICE: _clk_stm32_enable_core: if (parent != CLK_IS_ROOT)
NOTICE: _clk_stm32_enable_core: Calling clk_stm32_enable_call_ops
NOTICE: clk_stm32_enable_call_ops: Already enabled with id = 1
NOTICE: _clk_stm32_enable_core: Increase priv->gate_refcounts[1] from 0 to 1
NOTICE: _clk_stm32_enable: CLK Unlock: 0
NOTICE: _clk_stm32_enable: CLK Lock
NOTICE: _clk_stm32_enable_core: Increase priv->gate_refcounts[2] from 1 to 2
NOTICE: _clk_stm32_enable: CLK Unlock: 0
NOTICE: _clk_stm32_enable: CLK Lock
NOTICE: _clk_stm32_enable_core: Increase priv->gate_refcounts[3] from 1 to 2
NOTICE: _clk_stm32_enable: CLK Unlock: 0
NOTICE: _clk_stm32_enable: CLK Lock
NOTICE: _clk_stm32_enable_core: Increase priv->gate_refcounts[4] from 1 to 2
NOTICE: _clk_stm32_enable: CLK Unlock: 0
NOTICE: _clk_stm32_enable: CLK Lock
NOTICE: _clk_stm32_enable_core: if (parent != CLK_IS_ROOT)
NOTICE: _clk_stm32_enable_core: Calling clk_stm32_enable_call_ops
NOTICE: clk_stm32_enable_call_ops: Enabling with id = 5
ERROR: failed to enable clock id: 5
BACKTRACE: START: clk_stm32_enable_call_ops
0: EL3: 0xe017bac
1: EL3: 0xe01bf04
2: EL3: 0xe01bfb4
3: EL3: 0xe01c060
4: EL3: 0xe01c3ac
5: EL3: 0xe01dd0c
6: EL3: 0xe029c10
7: EL3: 0xe0170dc
BACKTRACE: END: clk_stm32_enable_call_ops
PANIC at PC : 0x000000000e01bf0c
2026-02-12 1:33 PM
Hi @PatrickF
I just want to say that I made an if-statement that check if the LSE is disabled. If they are disabled, it should only print out a warning and not call the panic function.
I think that the ST's tf-a assumes that both LSE and HSI should be active.
To reproduce this:
1. Remove the LSE crystal from DK/EV board
2. Disable LSE in CubeMX
3. Recompile new OpenSTLinux
4. Boot
5. View the early boot log
2026-04-10 3:36 AM - edited 2026-04-10 3:41 AM
Hello @DMårt
Thank you for your feedback, a patch is now available from OSTL DV6.1.1. It deactivates the external oscillator when not available, and prevents panic. It applies for STM32MP2xx and STM32MP1xx product familes.
For reference: https://community.st.com/t5/stm32-mpus-products-and-hardware/stm32mp135a-needs-an-lse-meta-st-stm32mp/m-p/858884#M15494
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.