2025-04-01 5:32 AM - edited 2025-04-01 5:32 AM
Hi ST community!
I am porting our Yocto bsp to the latest st scarthgap (openstlinux-6.6-yocto-scarthgap-mpu-v25.03.19) for our custom modules based on a stm32mp157c. When I source the Yocto SDK, the error is shown:
[SDK ERROR] Issue to optee export-user_ta directory
My main issue is that I cannot recompile optee (4.0.0-stm32mp-r1.2) outside of yocto:
make PLATFORM=stm32mp1 CFG_EMBED_DTB_SOURCE_FILE=<our-devkit>.dts CFG_TEE_CORE_LOG_LEVEL=2 O=build all
...
arm-poky-linux-gnueabi-ld.bfd: cannot find libgcc.a: No such file or directory
I have tried to pass the sysroot on the command line (CFLAGS, LDFLAGS, ...) but nothing worked!
Thanks for the pointers!
2025-04-10 4:11 PM - edited 2025-04-10 4:38 PM
I got this one fixed after changing the appended value to BOOTSCHEME_LABELS from "opteemin" to "optee". You will find this line in the machine configuration file of your custom board ( meta-st/meta-st-stm32mp-addons/conf/machine/).
After updating this don't forget to regenerate and re-install the SDK.
2025-04-15 2:53 AM - edited 2025-04-15 2:53 AM
Thanks for your input, I will give it a try! But what if I really want "opteemin"?
2025-04-15 4:26 PM
That's something I have not tried yet but if you look at the machine configuration file stmm32mp1.conf (meta-st/meta-st-stm32mp/conf/machine) BOOTSCHEME_LABELS is set to optee + opteemin + fastboot-opteemin + fastboot. I'm assuming for now we just have to always include optee for some reason.
2025-05-11 6:04 AM
Hey,
I tried your solution but it didn't work for me. Switching to the optee version had the same problem. I was using the Distribution-package (open Embedded build).
2025-05-12 10:52 AM
Hi cwei2010
Could you please provide more details as I already tested both of my suggestions are working.
2025-05-12 11:34 PM
Hi,
I checked again and found that switching to optee does work while building the default image (st-image-weston). However, I was using images like core-image-full-cmdline from meta layer so it couldn't get fixed from that. It pointed to somewhere, though, thanks a lot.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.