2025-06-18 1:37 AM - edited 2025-06-18 1:39 AM
Dear ST Developer Support,
I want to enable LVDS panel on STM32MP257F-EV1 based on Android OS.
I tried to modify device tree stm32mp257f-ev1.dts and stm32mp257f-ev1-overlay.dts to enable LVDS panel.
But I could not enable it. When I revert the device fdt file, I saw that the LVDS related device tree nodes
lvds
panel-lvds
panel-lvds-backlight
display-controller
status were "disabled".
In stm32mp257f-ev1.dts and stm32mp257f-ev1-overlay.dts file, the LVDS related device note are status="okay".
So, I confuse on this problem. Maybe somewhere dts overlay this device node, but I cannot find it.
Would you help me solve this problem?
Thanks.
Solved! Go to Solution.
2025-06-30 8:35 PM
Hi Philippe,
Yes, I just modify the panel_lvds node to fit my LVDS panel timing spec.
panel_lvds: panel-lvds {
compatible = "edt,etml0700z9ndha", "panel-lvds";
enable-gpios = <&gpiog 15 GPIO_ACTIVE_HIGH>;
backlight = <&panel_lvds_backlight>;
status = "okay";
width-mm = <261>;
height-mm = <163>;
data-mapping = "vesa-24";
panel-timing {
clock-frequency = <69900000>;
hactive = <1280>;
vactive = <800>;
hfront-porch = <72>;
hback-porch = <200>;
hsync-len = <128>;
vfront-porch = <3>;
vback-porch = <22>;
vsync-len = <6>;
};
port {
lvds_panel_in: endpoint {
remote-endpoint = <&lvds_out0>;
};
};
};
I have a question. if the lvds panel is disconnect, the ltdc and lvds status would show disabled?
Thanks.
2025-07-02 1:13 AM
Hi,
I did again some tests by modifying the panel-timing section to check if modifications are taken into account.
Be sure to use this command line to really update your image with your new dtb:
build_kernel ; build_kernel -i; make -j8
If screen is still black, timing might not be good (?)
To get more info on your LVDS connection, you can use "modetest" tool :
https://wiki.st.com/stm32mpu/wiki/DRM_KMS_overview#modetest_-28DRM-2FKMS_test_tool-29
For Android, I give you a few quick tips to use this binary as it is not installed by default:
cd external/libdrm/tests/modetest
mm
adb root
adb remount (takes a while sometimes)
adb push ./out/soong/.intermediates/external/libdrm/tests/modetest/modetest/android_arm64_armv8-a/modetest /vendor/bin/.
When LVDS is connected, you should get this "/vendor/bin/modetest" output on target:
id crtc type possible crtcs possible clones
31 0 DSI 0x00000001 0x00000001
33 44 LVDS 0x00000001 0x00000002
...
34 33 connected LVDS-1 156x92 1 33
modes:
index name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot
#0 1024x600 ...
Hope this can help you.
Philippe.
2025-07-02 2:47 AM
Hi Philippe,
I confuse a question. If the lvds panel is disconnect or connect other lvds panel, the ltdc and lvds status become "disabled"?
root@stm32mp2-e3-df-42:~# cat /proc/device-tree/soc@0/bus@42080000/display-controller@48010000/status
disabled
root@stm32mp2-e3-df-42:~# cat /proc/device-tree/soc@0/bus@42080000/lvds@48060000/status
disabled
root@stm32mp2-e3-df-42:~# cat /proc/device-tree/panel-lvds/status
disabledI found a situation, I use the same dtb, I connect the B-LVDS7-WSVGA panel, the lvds status would show "okay".
And I can see lvds driver log in dmsg, which I add some debug message in lvds driver.
But, when I disconnect lvds panel or connect other lvds panel, the lvds status would become "disabled".
Besides, the lvds driver would not probe in kernel. I cannot see any debug message which I added.
2025-07-02 7:31 AM
Hi,
I just got this information that uboot needs to be modified in case another LVDS panel is used.
Otherwise uboot will desactivate the LVDS DT node and we won't be able to get the driver working.
I will come back to you tomorrow with more explanation about necessary uboot patches.
BR,
Philippe.
2025-07-03 1:32 AM
Hi,
to modify uboot/bootloader, you need to follow this documentation:
https://wiki.st.com/stm32mpu/wiki/How_to_build_bootloaders_for_Android
And in order to use another LVDS screen than the standard one (etml0700z9ndha) delivered with Eval board, you have comment the following section in
"./device/stm/stm32mp2-bootloader/u-boot-stm32mp2/board/st/stm32mp2/stm32mp2.c" file (line 784)
//if (board_is_stm32mp257_eval()) {
// ret = fixup_stm32mp257_eval_panel(blob);
// if (ret)
// log_err("Error during panel fixup ! (%d)\n", ret);
//}
This will avoid to disable the DT node when another LVDS screen is used.
As explained in documentation, rebuild bootloader (build_bootloader), update it (build_bootloader -i), build full image (make -j) and reflash (flash-device).
Let me know if you have trouble,
BR,
Philippe.
2025-07-07 10:15 PM
Hi Philippe,
After I modified u-boot "stm32mp2.c" file, the LVDS panel can work. Thank your help!
But, I find another problem. The LVDS panel can bring up on android, it cannot show the ST logo system logo in u-boot and kernel boot up phase. How to enable the boot up logo on u-boot and kernel phase?
2025-08-01 12:53 AM
@PPAGE.13
I'm new to embedded linux, but i need a 10" display, for Yocto based Linux setup,
Currently i have a 7" display the one which i got with EVK (stm32mp257f-ev1)
https://mjmwired.net/kernel/Documentation/devicetree/bindings/display/panel/panel-lvds.yaml
in this lvds_panel.yaml file i saw
# Admatec 9904379 10.1" 1024x600 LVDS panel - admatec,9904379 - auo,b101ew05
# HannStar Display Corp. HSD101PWW2 10.1" WXGA (1280x800) LVDS panel - hannstar,hsd101pww2
So can i use these displays without modyfying any low level drivers or device tree.
Please at least give me a hint about selecting a display
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.