2020-08-13 7:18 AM
Error: failed to download Segment[0]
Error: failed to download the File
Error: Download partition 0x21 failed
Error: TSV flashing service failed
I am getting this error while flashing the image. I took the st-image-weston and deleted the ui and audio packages.
After doing this i m now experiencing these errors. But on repeatedly flashing again finally after 3,4 tries it get flashed.
I have seen other posts related to this that this error is somehow related to rootfs.
But i am not able to understand why removing graphics and audio packages affected the rootfs?
and what is the solution for thsi?
2020-08-18 4:26 AM
Hi @Hsn ,
Could you be more specific about the tool and version you use?
I expect it is CubeProgrammer, right? Which version?
What ecosystem are you working on? Latest 2.0?
Are you programming sdcard or other memory?
Thanks,
MIlan
2020-08-18 4:36 AM
Hi @mleo ,
Yes it is CubeProgrammer 2.4.0 and i am using it in ubuntu.
i am using this command to flash the sdcard.
STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv
and the distribution is openstlinux-5.4-dunfell-mp1-20-06-24
Thanks!
2020-08-25 5:59 AM
Hi @Hsn ,
Did you try latest CubeProgrammer 2.5?
What card do you use? There is an issue with Netac brand causing such error.
Please check.
Milan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.