STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to bitbake meta-toolchain-qt5

Hello everyone,I managed to build st-example-image-qt on my STM32MP157C-DK2 with some extra image features.Now i just want to run bitbake meta-toolchain-qt5 but the build end up with errors that i can't solve.I attached the output console when i try ...

AGATT.1 by Associate
  • 4204 Views
  • 2 replies
  • 0 kudos

Resolved! stm32_rtc: Prescaler config failed

Hi all,I'm developing a custom board based on STM32MP153 SoC, and I need to use the internal RTC. I also need to output its 32.768kHz reference clock from I8 pin.As stated at https://wiki.st.com/stm32mpu/wiki/RTC_device_tree_configuration, into the L...

Resolved! Xlib: I can not connect to the X server

Hi!I'm in search of a better GUI programming path :) Now trying Xlib.Here is a simple program from the Internet#include <stdio.h> #include <stdlib.h> #include <string.h> #include <errno.h> #include <X11/Xlib.h> extern int errno; int main( void ) {   ...

AShva.1 by Associate II
  • 2064 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.