2020-04-27 2:13 AM
I want to use a Winbond W25M02Gxx 256MByte (2x1Gbit) on MP157 QSPI1 port. It seems that the boot mode supports the use of Serial NAND Flash.
Anyone tried this?
2020-04-27 6:33 AM
Hello,
Although low level boot is already available (BootROM), Serial-NAND is not yet supported in STM32MPU Ecosystem (Linux, TF-A, uBoot, CubeMX, CubeProgrammer, etc..).
Please wait for future announcements.
2020-04-27 6:39 AM
That's a pity. If I read your message correctly: I can boot from NOR and/or NAND Flash from the embedded boot loader (depending on the BOOT0..2 pins. However, I need to add an eMMC or SDCARD to be able to bring up a system? Correct?
Is there a time line?
2020-04-27 7:43 AM
Today, you already have multiple options as boot sources :
see https://wiki.st.com/stm32mpu/wiki/Boot_chains_overview#Overview_2
Regarding Serial-NAND, you can only load FSBL (TF-A) from Serial-NAND to SYSRAM (this is done by the BootROM), but this TF-A and the remaining of the boot chain (uBoot, Linux) is not yet publicly available with Serial-NAND options.
For more details, please contact your nearest local ST support.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.