STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can i fix error with the gstreammer enum problem when trying bitbake st-image-weston

####Error messages are below..ERROR: gstreamer1.0-plugins-bad-1.14.4-r0 do_compile: oe_runmake failedERROR: gstreamer1.0-plugins-bad-1.14.4-r0 do_compile: Function failed: do_compile (log file is located at /home/kheng_sw/work/STM32MP1/Distribution-P...

SKim.12 by Associate II
  • 2928 Views
  • 3 replies
  • 0 kudos

stm32mp157a-dk2, Qt application crashes with a “Segmentation Fault�? when screen touched multiple times in quick succession.

Hi Guys,I’m having an issue connecting a touch screen to stm32mp157a-dk2. My Qt application crashes with a “Segmentation Fault�? when I touch the screen multiple times in quick succession.Has anyone else reported this problem before?Here is my setup:...

JSpra by Associate III
  • 1200 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP157x-EV1 stlinux device tree build

Hi. I have generated a full device tree for the EV1 to add I2C5 pins PA11/PA12 for external connector hookup to some of my I2C widgets using STM32CubeMX. I've place the generated .dts file from the kernel/ folder into <linux-source>/arch/arm/boot/dts...

ThePUP by Associate III
  • 2801 Views
  • 4 replies
  • 0 kudos

I use this : LSB Version: core-5.0-noarch:core-5.0-arm Distributor ID: openstlinux-weston Description: ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-openstlinux-20-02-19 Release: 2.6-openstlinux-20-02-19

I wan to install and develop userinterface programs using, tkinter and PyQt5 frameworks. but can not install both tkinter and pyqt5 , can you help please ?

Ahasa.1 by Associate
  • 1432 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.