2020-05-24 2:20 PM
Hi,
I have created a layer with my custom distro config and altered the conf/local.conf to point to this new distro. So far so good, everything worked as expected. Now comming back and I want to resource the environment with
source ./layers/meta-st/scripts/envsetup.shI got the following problem:
build@1f814fef97e6:/build$ source ./layers/meta-st/scripts/envsetup.sh
[HOST DISTRIB check]
Linux Distrib: Ubuntu
Linux Release: 18.04
[BUILD_DIR configuration]
1. build-openstlinuxeglfs-stm32mp1 - DISTRO is 'openstlinux-exut' and MACHINE is 'stm32mp1'
2. NEW - *** SET NEW DISTRO AND MACHINE BUILD CONFIG ***
Which one would you like? [build-openstlinuxeglfs-stm32mp1] 1
bash: [: -z: binary operator expected
Selected BUILD_DIR: build-openstlinuxeglfs-stm32mp1
[source layers/openembedded-core/oe-init-build-env][with previous config]
[ERROR] No 'openstlinux-exut.conf' file available in layers/meta-stI also got the same problem if I specified the build-directory as argument. Before creating the distro I had no problems with sourcing the file and also the file set has been working till I closed my console window.
There seems to be a problem with the layer configuration, which seems to be not set at the point the check runs, but I can never set the layer because I can not source the environment. I know the workaround is always to reset the distro in conf/local.conf but this is rather annoying.
Has anyone managed to define a custom distro in a separate layer and how was this rpoblem above solved?
2020-05-27 6:56 AM
Hi @Sven S.
Can you please share your custom layer and local.conf in order we can see what can cause such issue ?
Thanks
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.