STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DMA for USART

Hi all,I am trying assign DMA to USART3 channel on STM32MP1.I assigned it appropriately in the CubeMX but it looks like it was not able to auto-generate any code regarding the DMA assignment to the USART3.The device-tree bindings look pretty confusi...

NPal.2 by Senior
  • 2821 Views
  • 4 replies
  • 0 kudos

Resolved! PWM Limits for STM32MP1

Hi all,Referring to previous discussion I had.I just want understand what are the PWM limits for STM32MP1.I can't seem to generate PWM signal below 100ms. Any inputs will be appreciated.My target frequency is 1KHz.https://community.st.com/s/question/...

NPal.2 by Senior
  • 1816 Views
  • 1 replies
  • 0 kudos

Resolved! Maximum value of PWM period

Hi all,I have configured TIM1_CH3N as a pwm channel.I am trying to do some PWM functionality here.I am following current tutorial here. When i tried to provide a period of 10 sec it fails to take up the value. I get following error :root@stm32mp157a-...

NPal.2 by Senior
  • 3774 Views
  • 6 replies
  • 0 kudos

Resolved! SPI peripheral configuration help

Have been struggling to get SPI to work. I have been working in the engineering boot mode to try and trouble shoot my issues. I have configured PLL3 to run the MCU at 48MHz and the SPI peripheral kernel clk to run at 108MHz and selected the clock so...

Resolved! Kernel panic with poll/select syscalls on virtual UART devices to M4 core when M4 watchdog restarts

I am using 2 virtual UARTs as described in STM32MP1Cube Applications/OpenAMP/OpenAMP_TTY_echo example and watchdog for M4 core.Problem occurs when I using select or poll syscall to read from the device. Kernel panic occurs with following on dmesg log...

MMaje.1 by Associate
  • 13646 Views
  • 7 replies
  • 0 kudos

Resolved! Bringing up Ethernet on STM32MP153 with KSZ8081RNB in RMII mode and 25 MHz clock on ETH_CLK (no PHY Crystal)

Hello!I have an issue on a custom board with STM32MP153CAB and KSZ8081RNB.TF-A, FIP and kernel were built in Developer package. Linux distribution was built as startard configuration st-image-core in Distribution package.Clocks and device trees are c...

velaros by Associate III
  • 14639 Views
  • 21 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.