cancel
Showing results for 
Search instead for 
Did you mean: 

B‑LCDAD‑HDMI1 and STM32MP257F-EV1 and STM32MP2Starter

mfny
Associate III

Hello,

Would the B‑LCDAD‑HDMI1 adapter board work "out of the box" to connect a HDMI display to the STM32MP257F-EV1 running STM32MP2Starter ?

4 REPLIES 4
PatrickF
ST Employee

Hi @mfny 

yes, it should work if no other display/touch is connected to the board.

If needed, even if page was build for another board, this could help : https://wiki.st.com/stm32mpu/wiki/How_to_display_on_HDMI

 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

Searching on this forum shows there is an issue with the B‑LCDAD‑HDMI1 in that for some boards it does not mechanically mate with the host board making the connection very delicate, is this the case with the STM32MP257F-EV1 ?

Hi,

on STM32MP257F-EV1 and B‑LCDAD‑HDMI1 board, there is a mechanical hole on both board where you could put a 3mm screw with spacer.

Obviously, due to the size of the HDMI cables and the absence of enclosure, all cables should be handled with care to avoid bending or damages.

 

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
mfny
Associate III

Would you have a link to an example of "3mm screw with spacer" that would be suitable ?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.