2024-01-19 2:14 AM
Hello,
I'm working on the Wifi on the board B-U585I-IOT2A.
I'd like to connect 2 modules, including the microcontroller, to the same wifi so that they can communicate with each other.
I've made some research about Wifi MXCHIP EMW3080 and example HTTP_IOT_HTTPSERVER but i still not succeed to connect any network by taking parts of the code
Has anyone ever encountered this problematic before ?
could the lwip library be useful?
Thanks you for your help.
Solved! Go to Solution.
2024-02-01 1:55 AM
If I remember correctly , IOT_HTTP_WEBSERVER on B-U585I-IOT02A is based on FreeRTOS and LwIP for network stack.
We don't have lots of examples for LwIP on B-U585I-IOT02A.
The middleware on STM32U5 is based on ThreadX and NetXDuo network stack.
You can find network examples in STM32 Cube U5 in STM32CubeU5/Projects/B-U585I-IOT02A/Applications/NetXDuo at main · STMicroelectronics/STM32CubeU5 · GitHub
TCP_Echo_Client is an example of raw TCP connection.
There is no example for websocket protocol.
2024-01-26 6:06 AM
Hello
Could you give more details ?
What do you mean by "module" ? module = "B-U585I-IOT02A board" ?
"to the same wifi" : do you mean same WiFi Access Point ? what is it ? what is the security configuration ? WPA2 ?
What kind of communication do you want to do between the two "modules" ? which protocol ?
"not succeed to connect any network by taking parts of the code" -> did you write your own application with parts of the code ?
2024-01-29 1:31 AM
Hello Guillaume,
Thanks for your response.
Yes, so we would like to connect a B-U585I-IOT02A board (which i called module in the first message) to a Wi-fi Access Point with Wi-fi configuration is WPA2. The second module will not be a STM32 board but a generic IoT device.
We would like to exchange data using a websocket.
Concerning our application, we wrote our own code using parts of IOT_HTTP_WEBSERVER.
We are looking for any documentation or other project that could help us.
Thanks in advance.
2024-02-01 1:55 AM
If I remember correctly , IOT_HTTP_WEBSERVER on B-U585I-IOT02A is based on FreeRTOS and LwIP for network stack.
We don't have lots of examples for LwIP on B-U585I-IOT02A.
The middleware on STM32U5 is based on ThreadX and NetXDuo network stack.
You can find network examples in STM32 Cube U5 in STM32CubeU5/Projects/B-U585I-IOT02A/Applications/NetXDuo at main · STMicroelectronics/STM32CubeU5 · GitHub
TCP_Echo_Client is an example of raw TCP connection.
There is no example for websocket protocol.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.