2023-01-23 3:41 AM
I bought the P-NUCLEO-LRWAN3 STM32 Nucleo starter pack for LoRa and it says that if the NUCLEO-LO73RZ board's serial number is within a certain range, which it is, the board must be updated with a new firmware before use. However, the link provided only takes me to the LoRaWAN software expansion for STMCube. So, where can I get the new firmware that I must update the board with?
Solved! Go to Solution.
2023-01-23 3:59 AM
Hello @ABell.5 ,
Welcome to the Community :)
You are looking for I-CUBE-LRWAN STM32Cube Expansion Package (UM2073 UM2587).
When your question is answered, please close this topic by choosing Select as Best.
Imen
2023-01-23 3:55 AM
no idea aboput the lorawan boards.
But if they are anything like their BLE stm32WB boards you update the radio firmware with stmcubeProgrammer
Edit: they are completely different.
I believe they are supposed to be updated via UART?
2023-01-23 3:59 AM
Hello @ABell.5 ,
Welcome to the Community :)
You are looking for I-CUBE-LRWAN STM32Cube Expansion Package (UM2073 UM2587).
When your question is answered, please close this topic by choosing Select as Best.
Imen
2023-01-23 4:43 AM
The UM2073 is the right document for the STM32CubeExpansion_LRWAN_V2.1.0 and not the UM2587.
Thank you
2023-01-23 5:02 AM
Sorry! your are right, UM2073 (not UM2587)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.