2019-03-14 8:57 AM
I have got an STM32WB55 DK and i would like to use it with the CubeMonitor-RF.
I flashed the image for the co-processor but i am not sure which firmware for the main processor. I flashed the BLE Transparent Mode Application Firmware but the CubeMonitor-RF can not connect to the UART.
Thanks for your support!
2019-08-04 12:20 AM
It May be caused by failure in memory recognition system in CubeProg (if it's based on serial or other number hardcoded in bootloader)
Is it possible to flash radio binary via SWD?
I have holidays, so I can check it after week.
2019-08-11 4:20 PM
I've tried and it failed. Also my dongle is recognized in Device Manager.
During stack upgrade 256 kiBytes of memory are shown.
USB Dongles have 1MiB
Log below:
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in FS Mode
SN : 205E38773036
FW version : 0x011a
Device ID : 0x0495
Device name : STM32WBxx
Flash size : 256 KBytes
Device type : MCU
Device CPU : Cortex-M0+/M4
Download firmware image at address 0x80cc000 ...
Memory Programming ...
Opening and parsing file: stm32wb5x_BLE_Stack_fw.bin
File : stm32wb5x_BLE_Stack_fw.bin
Size : 162908 Bytes
Address : 0x080CC000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [204 243]
Download in Progress:
██████████████████████████████████████████████████ 100%
File download complete
Time elapsed during download operation: 00:00:01.765
Verifying ...
Read progress:
██████████████████████████████████████████████████ 100%
Download verified successfully
RSS state is RSS_SERVICE_ONGOING
RSS status is RSS_IMAGE_NOT_FOUND
RSS state is RSS_IDLE
RSS status is RSS_NO_ERROR
Firmware Upgrade process started ...
Updating firmware ...
Waiting for firmware upgrade end
RSS state is WIRELESS_STACK_UPGRADE_ONGOING
RSS status is RSS_IMAGE_NOT_FOUND
Warning: Firmware upgrade Error!Retrying...
Retry -- 0
etc.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.