2023-04-17 6:36 AM
How can i program stm32wle5ccu6 with st-link which is on the nucleo stm32g474ret6 or is it possible?
2023-04-17 6:51 AM
Hello,
Sure it is possible, we must remove the solder bridge going from nucleo stlink to imbedded STM32G4 and verify that the target board is also supplied at 3.3V as the nucleo G474 is.
Regards,
Simon
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.