2025-12-02 6:55 AM
When generating code im getting two erros:
In timer_if.c:
in LoraMac.c:
I've been trying to look for some answers but i couldn't really find something useful.
If someone can help i'd really appreciate it.
Regards.
Solved! Go to Solution.
2025-12-02 11:16 AM
Hello @Doug3 and welcome to the Community,
I recommend you refer to the ready-to-use LoRaWAN End-Node example which is available within STM32CubeWL firmware package: STM32CubeWL/Projects/NUCLEO-WL55JC/Applications/LoRaWAN at main · STMicroelectronics/STM32CubeWL · GitHub
Then, import and adapt the example using STM32CubeMX and STM32CubeIDE, following the guides for configuration and customization: How to import STM32CubeWL repository projects onto... - STMicroelectronics Community
The following wiki page contains information such as, application examples, document references, and tips related to STM32 LoRaWAN: Introduction to LoRaWAN® - stm32mcu
2025-12-02 11:16 AM
Hello @Doug3 and welcome to the Community,
I recommend you refer to the ready-to-use LoRaWAN End-Node example which is available within STM32CubeWL firmware package: STM32CubeWL/Projects/NUCLEO-WL55JC/Applications/LoRaWAN at main · STMicroelectronics/STM32CubeWL · GitHub
Then, import and adapt the example using STM32CubeMX and STM32CubeIDE, following the guides for configuration and customization: How to import STM32CubeWL repository projects onto... - STMicroelectronics Community
The following wiki page contains information such as, application examples, document references, and tips related to STM32 LoRaWAN: Introduction to LoRaWAN® - stm32mcu
2025-12-02 12:09 PM
Hello @Doug3
For the first error on the timer_if.c, it seems that you have create the user constant RTC_N_PREDIV_S as RTC_PRER_PREDIV_S so, the code can’t find this user constant (RTC_N_PREDIV_S). Make sure it is correctly declared.
For the second error on the LoraMac.c, this is a known issue on the STM32CubeWL, temporary solution is to select the LoRaWAN Link Layer V1.0.4 and not the LoRaWAN Link Layer V1.0.3.
Best Regards.
II
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.